Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Where's the board definition install for vivado 2018?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 371 subscribers
  • Views 933 views
  • Users 0 members are here
Related

Where's the board definition install for vivado 2018?

shanedora
shanedora over 7 years ago

I've installed vivado 2018 and I'm following the tutorials under the microzed section on your site. I'm extremely confused on where to begin so I choose to start with the first tutorial which is building a hardware platform.

In the "Experiment Setup" section of the tutorial it gives the software used to test this reference design being...

Windows 7
Xilinx Vivado 2016
Board Definition Install for Vivado 2015.3, 2015.4, 2016.1, 2016.2, 2016.4 and 2017.

I'm using a CentOS7 systems and have installed Xilinx Vivado 2018. On your site there are downloads for Board Definition belonging to the MicroZed. Which one do I choose...all of them? Why isn't there a 2018 version? Will the older ones work with Vivado 2018? What is this Board Definition?

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 7 years ago

    The existing board definition also works in 2018. The Board Definition or Board File is defined in Xilinx UG895 -- https://www.xilinx.com/support/documentation/sw_manuals/xilinx2018_2/ug895-vivado-system-level-design-entry.pdf

    "The Board file uses an XML format to define information about system-level boards that use or include XilinxRegistered devices. The information contained in the Board file can be used by the VivadoRegistered Design Suite, and Vivado IP integrator, to facilitate and validate connection of the Xilinx device to the board."

    That same document also provides detailed instructions on how to install board definition files.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer