Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Debugging startup
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 426 views
  • Users 0 members are here
Related

Debugging startup

e14 Contributor
e14 Contributor over 13 years ago

Sorry if this is covered elsewhere, but I've not found it yet. So I got my Zedboard (Yay!) but no luck on the getting started stuff.

Plugged in the board, plugged in the USB, installed the Cypress USB serial port, can see that on my Win7/64 machine. Turn the board on, green power light comes on and then nothing. No '15 seconds later the blue "done" light' nothing on the serial port as far as Putty can see, SD card (which was inserted when I got it) seems to be correctly inserted etc.

Currently looking for the SD card image to consider re-imaging the card but if someone reads this before then and says "Oh yeah you also need to do ..." that would be great as well.

--Chuck

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    So I looked at the SD CARD that came with the board and it had a README file, that file included a description of how the jumpers should be set on the board. A bunch of the jumpers on the board were not correct, in particular MIO4,5 to 3V3 (rather than ground) VADJ to 1V8 (it was on 2V5) and JP6 needed to be jumpered but there was no jumper on the board so I took one out of my spares. Once I did that and powered it up it worked as expected, blue LED came on , OLED display lit up with Digilent logo and presumably the VGA and HDMI things are working too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    So I looked at the SD CARD that came with the board and it had a README file, that file included a description of how the jumpers should be set on the board. A bunch of the jumpers on the board were not correct, in particular MIO4,5 to 3V3 (rather than ground) VADJ to 1V8 (it was on 2V5) and JP6 needed to be jumpered but there was no jumper on the board so I took one out of my spares. Once I did that and powered it up it worked as expected, blue LED came on , OLED display lit up with Digilent logo and presumably the VGA and HDMI things are working too.