Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Confused about ps7_init.h/.c
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 358 subscribers
  • Views 1133 views
  • Users 0 members are here
Related

Confused about ps7_init.h/.c

Former Member
Former Member over 9 years ago

Hi,

I am confused about the purpose of the ps7_init.h/.c/.tcl files. Currently I am just using the hello_world example on Zedboard. I have successfully run this via JTAG, QSPI, and SD card without issues.

However, I see in the platform.c files that it indicates if I want to run this outside of the SDK I should #include ps7_init.h and call ps7_init() in init_platform().

However if I add the include and call ps7_init() it hangs indefinitely during the DDR initialization.

My questions are:
1. What does it mean by running outside of the SDK? I have successfully run the standard hello_world w/o calling ps7_init from the SD card and QSPI, this seems to be outside the SDK.
2. When/why do I need to call ps7_init()? The hello_world example seems to run perfectly fine without it.
3. What's the relationship between ps7_init.tcl and ps7_init.h/.c?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 9 years ago

    Thank you. I see in the FSBL that I have made (just using the FSBL example in the SDK) that ps7_init() is one of the first functions called.

    This indicates to me that I should not need to call it again in my bare metal application. But why then does the hello_world example say that I should uncomment it if I'm running from the SD/QSPI?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    Thank you. I see in the FSBL that I have made (just using the FSBL example in the SDK) that ps7_init() is one of the first functions called.

    This indicates to me that I should not need to call it again in my bare metal application. But why then does the hello_world example say that I should uncomment it if I'm running from the SD/QSPI?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    All I see is a comment in the platform.c about ps7_init.h, not ps7_init.c. This is a question you would need to ask Xilinx, perhaps on one of their community forums.

     

    -Gary