Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General U-Boot Issues
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 372 subscribers
  • Views 668 views
  • Users 0 members are here
Related

U-Boot Issues

e14 Contributor
e14 Contributor over 13 years ago


I'm following the instructions on the Build U-Boot wiki (www.wiki.xilinx.com/Build+U-Boot) and am running into some issues.

The first errors kept saying that it couldn't find the command for "arm-linux-ar" or "arm-linux-gcc", etc. I fixed this by making a soft link to "arm-linux-gnueabi-ar", "arm-linux-gnueabi-gcc", etc. (for example: sudo ln -s /usr/bin/arm-linux-gnueabi-gcc /usr/bin/arm-linux-gcc). That made everything compile correctly (with no errors) when I executed the "make -j zynq_zed" command.

However, the wiki says that after this completes, the u-boot elf file should be located in the top level source directory, and that the mkimage utility is created in the tools directory. This is not the case. Neither file is anywhere to be found... I'm not getting any errors during the build, and I'm confused on why this isn't working... Please help!

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Instead of using hard/soft-links you could use set CROSS_COMPILE:
    export CROSS_COMPILE=arm-xilinx-linux-gnueabi-
    or
    export CROSS_COMPILE=arm-linux-gnueabi-

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the reply vanmierlo.

    The problem was that I didn't have the cross compile toolchain installed from code sourcery. I had read somewhere that it came with the Xilinx design suite, but it doesn't. I found the link to install the tools on one of the speedway labs.

    When I tried to compile the kernel with arm-linux-gnueabi-, it would seize up and I'd have to restart. For some reason, the arm-xilinx-linux-gnueabi- is a little smoother for kernel corss-compilation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the reply vanmierlo.

    The problem was that I didn't have the cross compile toolchain installed from code sourcery. I had read somewhere that it came with the Xilinx design suite, but it doesn't. I found the link to install the tools on one of the speedway labs.

    When I tried to compile the kernel with arm-linux-gnueabi-, it would seize up and I'd have to restart. For some reason, the arm-xilinx-linux-gnueabi- is a little smoother for kernel corss-compilation.