Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Boot Problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 836 views
  • Users 0 members are here
Related

Boot Problem

e14 Contributor
e14 Contributor over 13 years ago

Hi all,

I have a ZedBoard and I'd like to recompile u-boot and kernel from sources. These are the steps that I follow:
1. create a new PlanAhead project (RTL project) selecting ZedBoard
2. in the "Sources View" select "Design Sources" and then Add Sources
  a. select Add or Create Embedded Sources
  b. select Create Sub-Design (name = system)
3. In XPS create a base system using the Wizard
  a. select AXI system
  b. select ZedBoard
  c. BTNs_5Bits LEDs_8Bits and SWs_8Bits included in Processing System7
4. Close XPS tool
5. In PlanAhead create top HDL
6. Select Generate Bitstream in "Program and Debug" section of Flow Navigator

@@ I got these warnings: @@
[Constraints 18-5] Cannot loc instance 'processing_system7_0_PS_PORB_IBUF' at site B5, Site location is not valid [C:/Xilinx/Projects/ZedBoard/ZedBoard.srcs/sources_1/edk/system/implementation/system_processing_system7_0_wrapper.ncf:157]
[Constraints 18-5] Cannot loc instance 'processing_system7_0_PS_SRSTB_IBUF' at site C9, Site location is not valid [C:/Xilinx/Projects/ZedBoard/ZedBoard.srcs/sources_1/edk/system/implementation/system_processing_system7_0_wrapper.ncf:158]
[Constraints 18-5] Cannot loc instance 'processing_system7_0_PS_CLK_IBUF' at site F7, Site location is not valid [C:/Xilinx/Projects/ZedBoard/ZedBoard.srcs/sources_1/edk/system/implementation/system_processing_system7_0_wrapper.ncf:159]
7. Select Export -> Hardware to SDK and starts SDK tool
8. Create a new Zynq FSBL project and related SDK (zed_fsbl_0 project name)
9. Compile FSBL project
10. Compile u-boot cloning the GIT repository
  $ make CROSS_COMPILE=arm-xilinx-linux-gnueabi- zynq_zc70x_config
  $ make CROSS_COMPILE=arm-xilinx-linux-gnueabi-
11. Generate the new BOOT.BIN file using:
  zed_fsbl_0.elf  (binary)
  system.bit      (bitstream)
  u-boot.elf      (binary)
12. Copy the BOOT.BIN file into the SD card of the board

On boot I got this error:

Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0
[    0.000000] Linux version 3.3.0-digilent-12.07-zed-beta (tinghui.wang@DIGILENT_LINUX) (gcc versi2
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Memory policy: ECC disabled, Data cache writealloc
[    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space
[    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space
[    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space
[    0.000000] PERCPU: Embedded 7 pages/cpu @c1489000 s5696 r8192 d14784 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125824
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x800000,8M early0
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 240MB 256MB = 496MB total
[    0.000000] Memory: 489856k/489856k available, 34432k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc042f040   (4253 kB)
[    0.000000]       .init : 0xc0430000 - 0xc0456640   ( 154 kB)
[    0.000000]       .data : 0xc0458000 - 0xc0485dc0   ( 184 kB)
[    0.000000]        .bss : 0xc0485de4 - 0xc049d734   (  95 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Verbose stalled-CPUs detection is disabled.
[    0.000000] NR_IRQS:128
[    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43
[    0.000000] Console: colour dummy device 80x30
[    0.000000] Calibrating delay loop... 1594.16 BogoMIPS (lpj=7970816)
[    0.090000] pid_max: default: 32768 minimum: 301
[    0.090000] Mount-cache hash table entries: 512
[    0.090000] CPU: Testing write buffer coherency: ok
[    0.090000] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.100000] smp_twd: clock not found: -2
[    0.100000] Calibrating local timer... 399.36MHz.
[    0.170000] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[    0.170000] Setting up static identity map for 0x2f8d48 - 0x2f8d7c
[    0.270000] CPU1: Booted secondary processor
[    0.310000] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.310000] Brought up 2 CPUs
[    0.310000] SMP: Total of 2 processors activated (3188.32 BogoMIPS).
[    0.320000] devtmpfs: initialized
[    0.320000] ------------[ cut here ]------------
[    0.320000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.330000] Modules linked in:
[    0.330000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4)
[    0.340000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+)
[    0.350000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/)
[    0.360000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x)
[    0.360000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.370000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.380000] ---[ end trace 1b75b31a2719ed1c ]---
[    0.380000] ------------[ cut here ]------------
[    0.390000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.390000] Modules linked in:
[    0.390000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4)
[    0.400000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+)
[    0.410000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/)
[    0.420000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x)
[    0.430000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.430000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.440000] ---[ end trace 1b75b31a2719ed1d ]---
[    0.440000] NET: Registered protocol family 16
[    0.460000] L310 cache controller enabled
[    0.460000] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B
[    0.460000] registering platform device 'pl330' id 0
[    0.470000] registering platform device 'arm-pmu' id 0
[    0.470000]
[    0.470000] ###############################################
[    0.480000] #                                             #
[    0.480000] #                Board ZED Init               #
[    0.480000] #                                             #
[    0.490000] ###############################################
[    0.490000]
[    0.500000] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.500000] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.530000] xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000
[    0.540000] bio: create slab <bio-0> at 0
[    0.540000] gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops
[    0.540000] xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000
[    0.550000] Unhandled fault: imprecise external abort (0x406) at 0x00000000
[    0.550000] Internal error: : 406 [#1] PREEMPT SMP
[    0.550000] Modules linked in:
[    0.550000] CPU: 0    Tainted: G        W     (3.3.0-digilent-12.07-zed-beta #2)
[    0.550000] PC is at __rcu_read_unlock+0x0/0x4c
[    0.550000] LR is at release_task+0x38/0x438
[    0.550000] pc : [<c005bd60>]    lr : [<c00206e4>]    psr: 60000013
[    0.550000] sp : d80f7f90  ip : d80f6010  fp : 00000000
[    0.550000] r10: 00000001  r9 : d80f7fbc  r8 : d811293c
[    0.550000] r7 : d811293c  r6 : c0466364  r5 : c0466368  r4 : d8112800
[    0.550000] r3 : d8112800  r2 : 00000001  r1 : 00000011  r0 : 00000000
[    0.550000] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
[    0.550000] Control: 18c5387d  Table: 0000404a  DAC: 00000015
[    0.550000] Process kworker/u:0 (pid: 336, stack limit = 0xd80f62f0)
[    0.550000] Stack: (0xd80f7f90 to 0xd80f8000)
[    0.550000] 7f80:                                     d8112800 00000001 d8112800 00000001
[    0.550000] 7fa0: 00000000 d811293c d811293c d80f7fbc 00000001 c0021f98 00000000 d80f7fbc
[    0.550000] 7fc0: d80f7fbc d8112984 d8348540 d8348554 fffffffe 00000013 00000000 00000000
[    0.550000] 7fe0: 00000000 c002ffa4 d8348540 c002fe8c c000dfcc c000dfcc c0101009 69452425
[    0.550000] [<c005bd60>] (__rcu_read_unlock+0x0/0x4c) from [<00000001>] (0x1)
[    0.550000] Code: e121f007 e8bd85f8 03ff0100 c04673c0 (e92d4010)
[    0.560000] ---[ end trace 1b75b31a2719ed1e ]---
[    0.560000] Unhandled fault: imprecise external abort (0x406) at 0x00000000
[    0.560000] Fixing recursive fault but reboot is needed!
[    0.560000] Internal error: : 406 [#2] PREEMPT SMP
[    0.560000] Modules linked in:
[    0.560000] CPU: 0    Tainted: G      D W     (3.3.0-digilent-12.07-zed-beta #2)
[    0.560000] PC is at kernel_thread_helper+0x0/0x10
[    0.560000] LR is at kernel_thread_helper+0x0/0x10
[    0.560000] pc : [<c000dfbc>]    lr : [<c000dfbc>]    psr: 00000093
[    0.560000] sp : d843bff8  ip : 00000000  fp : 00000000
[    0.560000] r10: 00000000  r9 : 00000000  r8 : 00000000
[    0.560000] r7 : 00000013  r6 : c000dfcc  r5 : c002fe8c  r4 : d8348380
[    0.560000] r3 : 00000000  r2 : 00000000  r1 : 00000000  r0 : 00000000
[    0.560000] Flags: nzcv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment kernel
[    0.560000] Control: 18c5387d  Table: 0000404a  DAC: 00000015
[    0.560000] Process kworker/u:0 (pid: 339, stack limit = 0xd843a2f0)
[    0.560000] Stack: (0xd843bff8 to 0xd843c000)
[    0.560000] bfe0:                                                       03bb0014 50803f60
[    0.560000] Code: 11a00150 12000001 e12fff1e c02fa19c (e121f007)
[    0.570000] ---[ end trace 1b75b31a2719ed1f ]---
[    0.570000] SCSI subsystem initialized
[    0.580000] usbcore: registered new interface driver usbfs
[    0.580000] usbcore: registered new interface driver hub
[    0.590000] usbcore: registered new device driver usb
[    0.590000] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.600000] Switching to clocksource xttcpss_timer1
[    0.610000] NET: Registered protocol family 2
[    0.610000] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[    0.610000] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[    0.620000] TCP bind hash table entries: 16384 (order: 5, 196608 bytes)
[    0.620000] TCP: Hash tables configured (established 16384 bind 16384)
[    0.630000] TCP reno registered
[    0.630000] UDP hash table entries: 256 (order: 1, 8192 bytes)
[    0.640000] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[    0.640000] NET: Registered protocol family 1
[    0.650000] Trying to unpack rootfs image as initramfs...
[    0.650000] rootfs image is not initramfs (no cpio magic); looks like an initrd
[    0.680000] Freeing initrd memory: 8192K
[    0.690000] xscugtimer xscugtimer.0: ioremap fe00c200 to e0810200 with size 400
[    0.690000] pl330 dev 0 probe success
[    0.700000] msgmni has been set to 972
[    0.700000] io scheduler noop registered
[    0.700000] io scheduler deadline registered
[    0.700000] io scheduler cfq registered (default)
[    0.710000] e00   0.710000] console [ttyPS0] enabled, bootconsole disabled
[    0.710000] console [ttyPS0] enabled, bootconsole disabled
[    0.720000] xdevcfg f8007000.devcfg: ioremap f8007000 to e0814000 with size 1000
[    0.730000] [drm] Initialized drm 1.1.0 20060810
[    0.740000] brd: module loaded
[    0.750000] loop: module loaded
[    0.750000] xqspips e000d000.qspi: at 0xE000D000 mapped to 0xE0816000, irq=51
[    0.760000] GEM: BASEADDRESS hw: e000b000 virt: e0818000
[    0.760000] XEMACPS mii bus: probed
[    0.770000] eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
[    0.770000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    0.780000] usb_hcd_xusbps_probe: No OTG assigned!
[    0.780000] usb_hcd_xusbps_probe: OTG now assigned!
[    0.780000] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
[    0.790000] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
[    0.830000] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
[    0.850000] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
[    0.850000] hub 1-0:1.0: USB hub found
[    0.850000] hub 1-0:1.0: 1 port detected
[    0.860000] Initializing USB Mass Storage driver...
[    0.860000] usbcore: registered new interface driver usb-storage
[    0.870000] USB Mass Storage support registered.
[    0.870000] Xilinx PS USB Device Controller driver (Apr 01, 2011)
[    0.880000] mousedev: PS/2 mouse device common for all mice
[    0.880000] Unhandled fault: imprecise external abort (0x406) at 0x00000000
[    0.890000] Internal error: : 406 [#3] PREEMPT SMP
[    0.890000] Modules linked in:
[    0.890000] CPU: 1    Tainted: G      D W     (3.3.0-digilent-12.07-zed-beta #2)
[    0.900000] PC is at xiic_clear_rx_fifo+0x1c/0x2c
[    0.900000] LR is at xiic_reinit+0x98/0x124
[    0.910000] pc : [<c0208200>]    lr : [<c02082a8>]    psr: 60000013
[    0.910000] sp : d804fee8  ip : e0820000  fp : 00000058
[    0.920000] r10: 00000000  r9 : d8071818  r8 : d80b2808
[    0.920000] r7 : 00000000  r6 : d806c840  r5 : c0460454  r4 : d8071800
[    0.930000] r3 : e0820000  r2 : 00000000  r1 : 00000001  r0 : d8071800
[    0.930000] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel
[    0.940000] Control: 18c5387d  Table: 0000404a  DAC: 00000015
[    0.940000] Process swapper/0 (pid: 1, stack limit = 0xd804e2f0)
[    0.950000] Stack: (0xd804fee8 to 0xd8050000)
[    0.950000] fee0:                   00000000 d8071800 d80b2800 c02f1ca0 00000000 c0479cbc
[    0.960000] ff00: 00000000 d80b2808 c04997f4 c0479cbc c0479cbc 00000000 00000000 00000000
[    0.960000] ff20: 00000000 c0194988 c0194974 c0193a90 00000000 d80b2808 d80b283c c0479cbc
[    0.970000] ff40: 00000000 c0193bac c0479cbc c0193b4c 00000000 c0192660 d803c820 d80afa78
[    0.980000] ff60: c0479cbc d8406740 c046f1f8 c01933ac c03d74e1 00000001 00000000 c0479cbc
[    0.980000] ff80: c0443de4 00000000 00000013 00000000 00000000 c0194084 d804ffb8 c0443de4
[    0.990000] ffa0: 00000000 00000013 00000000 00000000 00000000 c000858c c0466524 00000000
[    1.000000] ffc0: c0466524 c013e910 c04545fc c0454900 c04545fc c000dfcc 00000013 00000000
[    1.000000] ffe0: 00000000 c043085c 00000000 00000000 c04307d8 c000dfcc c0905009 69452425
[    1.010000] [<c0208200>] (xiic_clear_rx_fifo+0x1c/0x2c) from [<c02082a8>] (xiic_reinit+0x98/0x12)
[    1.020000] [<c02082a8>] (xiic_reinit+0x98/0x124) from [<c02f1ca0>] (xiic_i2c_probe+0x100/0x230)
[    1.030000] [<c02f1ca0>] (xiic_i2c_probe+0x100/0x230) from [<c0194988>] (platform_drv_probe+0x14)
[    1.030000] [<c0194988>] (platform_drv_probe+0x14/0x18) from [<c0193a90>] (driver_probe_device+0)
[    1.040000] [<c0193a90>] (driver_probe_device+0xc8/0x184) from [<c0193bac>] (__driver_attach+0x6)
[    1.050000] [<c0193bac>] (__driver_attach+0x60/0x84) from [<c0192660>] (bus_for_each_dev+0x48/0x)
[    1.060000] [<c0192660>] (bus_for_each_dev+0x48/0x74) from [<c01933ac>] (bus_add_driver+0x98/0x2)
[    1.060000] [<c01933ac>] (bus_add_driver+0x98/0x214) from [<c0194084>] (driver_register+0xa0/0x1)
[    1.070000] [<c0194084>] (driver_register+0xa0/0x134) from [<c000858c>] (do_one_initcall+0x90/0x)
[    1.080000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    1.090000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    1.090000] Code: f57ff04f e590c000 e59c2104 f57ff04f (e6ef1072)
[    1.100000] ---[ end trace 1b75b31a2719ed20 ]---

I think that I miss some steps ... can anyone help me?

Do I need to recompile also the kernel and other elements?

Best Regards,
Alessandro.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 13 years ago

    Hi EvidenceSrl,

    Looks like you are still using the Digilent OOB Linux kernel.  It looks like you created your PL and PS design from scratch rather than from the source.  I also did not see any mention of modifying the device tree so you might be reusing the one from the OOB demo.  If that is the case then Linux is probably attempting to initialize some PL peripherals that are not instantiated in your from scratch PL design, which may cause the kernel to lock up during boot as shown in your console output.

    I can think of two ways to move you forward, each depending on where you want to focus your design energy.

    The first path is to obtain the Digilent sources for the PL design which can be found on the Digilent site:

    http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,1028&Prod=ZEDBOARD

    The second path would be to modify your device tree by slowly removing device listings (especially ones in the PL) until your Linux boots to the command prompt.

    You could also recompile the kernel, but that may not make much difference until you modify the device tree and reduce your platform description to something more basic that matches your PL hardware design.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to zedhed

    Hi,

    thanks for reply. I try to recompile the kernel from Xilinx repository using the xilinx_zynq_defconfig. On boot I receive this error:

    Error: unrecognized/unsupported machine ID (r1 = 0x1fb6ad84).

    Questions:
    - can I use the Xilinx kernel or I must use the Digilent kernel?
    - there is a default config for ZedBoard supported by Xilinx?

    Best Regards,
    Alessandro.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to zedhed

    Hi,

    thanks for reply. I try to recompile the kernel from Xilinx repository using the xilinx_zynq_defconfig. On boot I receive this error:

    Error: unrecognized/unsupported machine ID (r1 = 0x1fb6ad84).

    Questions:
    - can I use the Xilinx kernel or I must use the Digilent kernel?
    - there is a default config for ZedBoard supported by Xilinx?

    Best Regards,
    Alessandro.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi,
    I have exactly the same problem, I also get the machine ID error. The r1 value changes a little each time I restart and try again. It also prints out that the compatible machine ID is B32 (hex), which shows up in the source code for both u-boot and Linux in a few places (as decimal 3378).

    I've built u-boot and the kernel from Xilinx's git repo, 14.3 build2 trd.

    (I also tried 14.2, no luck)
    Using ZED board, zynq_zed_config for u-boot and and xilinx_zynq_defconfig for Linux.

    I've seen this error in one or two other locations too, including here:
    http://www.zedboard.org/content/recompile-linux-kernel

    I tried loading my fresh compiled fsbl&u-boot with the stock zedboard zImage, and it got a lot further. This leads me to believe that the problem is with the configuration of Linux.

    Thanks,
    Mark Garrison

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hello Mark,
    Did you ever solve your problem?  If so, what did you do?