Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General no PHY setup on Zedboard using petalinux 2014.2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 374 subscribers
  • Views 1380 views
  • Users 0 members are here
Related

no PHY setup on Zedboard using petalinux 2014.2

e14 Contributor
e14 Contributor over 11 years ago

I have made a simple Zedboard configuration using Vivado 2014.2 and Petalinux 2014.2 under SUSE enterprise. The configuration just has the switches, buttons and LEDu2019s.
After exporting things from Vivado I run through the following

petalinux-create --type project --template <CPU_TYPE> --name <PROJECT_NAME>
cd <directory which contains hardware description file>
petalinux-config --get-hw-description -p <plnx-proj-root>

I use the menu to select SD card booting then run;

petalinux-build

Finally I do;

petalinux-package --boot --fsbl <FSBL image> --fpga <FPGA bitstream> --uboot

After copying the BOOT.bin and image.ub files onto and SD card the board boots up and runs my little test app ok.

I tried ifconfig 192.168.1.3 and that was OK but I get no response from a ping on the Ethernet. Looking at the boot results is appears I have the following error
u201CConfiguring network interfaces... xemacps e000b000.ps7-ethernet: eth0: no PHY setupu201D

Apparently this means I have no Ethernet driver, so my question is simple, what do I have to change in the build configuration to get this driver built for the Zedboard?

Thanks in advance for your help

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Here is a forum post on the issue of MicroZed Ethernet LEDs that might be helpful:

     http://zedboard.org/content/ethernet-leds-constant-and-not-blinking

     

    As mentioned in that post the Marvell PHY data sheet is under an NDA (Non Disclosure Agreement). You can work with your local Avnet/Silica FAE to request access to the data sheet from Marvell.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bkamen
    0 bkamen over 11 years ago in reply to e14 Contributor

    Don't think I'll need it at this point as I ran some tests from my Managed switch and the LEDs seem to be ok.

    If I may offer the comment though, as I've been in this situation more than once and it's simply obnoxious for a company to sell development building blocks without all the relevant documentation.

    Thanks for your help though. (I've given up trying to get any direction from my FAE.)

    -Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bkamen
    0 bkamen over 11 years ago in reply to e14 Contributor

    Don't think I'll need it at this point as I ran some tests from my Managed switch and the LEDs seem to be ok.

    If I may offer the comment though, as I've been in this situation more than once and it's simply obnoxious for a company to sell development building blocks without all the relevant documentation.

    Thanks for your help though. (I've given up trying to get any direction from my FAE.)

    -Ben