Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Lab 9 cpu1 BSP difficulties
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 669 views
  • Users 0 members are here
Related

Lab 9 cpu1 BSP difficulties

e14 Contributor
e14 Contributor over 10 years ago

Has anyone been doing the SW Speedway series and gotten to the dual processor software development and encountered a problem with creating the second (cpu1) bsp? I get a flood of errors from LONG not being declared.

I had to truncate the error messages to not get labeled as spam.

xemacps_bdring.c:514:13: error: 'LONG' undeclared (first use in this function)
   Status = (LONG)(XST_FAILURE);
             ^
xemacps_bdring.c: At top level:
xemacps_bdring.c:552:1: error: unknown type name 'LONG'
LONG XEmacPs_BdRingToHw(XEmacPs_BdRing * RingPtr, u32 NumBd,
^
xemacps_bdring.c: In function 'XEmacPs_BdRingToHw':
xemacps_bdring.c:557:2: error: unknown type name 'LONG'
  LONG Status;
  ^
xemacps_bdring.c:560:13: error: 'LONG' undeclared (first use in this function)
   Status = (LONG)(XST_SUCCESS);
             ^

(truncated errors)

xemacps.h:780:1: error: unknown type name 'LONG'
LONG XEmacPs_SetTypeIdCheck(XEmacPs *InstancePtr, u32 Id_Check, u8 Index);
^
xemacps.h:782:1: error: unknown type name 'LONG'
LONG XEmacPs_SendPausePacket(XEmacPs *InstancePtr);
^
make[1]: *** [xemacps_sinit.o] Error 1
make[1]: Target `libs' not remade because of errors.
make: *** [ps7_cortexa9_1/libsrc/emacps_v3_1/src/make.libs] Error 2
"Running Make libs in ps7_cortexa9_1/libsrc/gpiops_v3_1/src"
make -C ps7_cortexa9_1/libsrc/gpiops_v3_1/src -s libs  "SHELL=CMD" "COMPILER=arm-xilinx-eabi-gcc" "ARCHIVER=arm-xilinx-eabi-ar" "COMPILER_FLAGS=  -O2 -c" "EXTRA_COMPILER_FLAGS=-g -DUSE_AMP=1"
"Compiling gpiops"
In file included from xgpiops.c:62:0:
xgpiops.h:115:28: fatal error: xplatform_info.h: No such file or directory
#include "xplatform_info.h"
                            ^
compilation terminated.
make[1]: *** [xgpiops.o] Error 1
In file included from xgpiops_g.c:41:0:
xgpiops.h:115:28: fatal error: xplatform_info.h: No such file or directory
#include "xplatform_info.h"
                            ^

compilation terminated.
make[1]: *** [xuartps_sinit.o] Error 1
make[1]: Target `libs' not remade because of errors.
make: *** [ps7_cortexa9_1/libsrc/uartps_v3_1/src/make.libs] Error 2
"Running Make libs in ps7_cortexa9_1/libsrc/usbps_v2_2/src"
make -C ps7_cortexa9_1/libsrc/usbps_v2_2/src -s libs  "SHELL=CMD" "COMPILER=arm-xilinx-eabi-gcc" "ARCHIVER=arm-xilinx-eabi-ar" "COMPILER_FLAGS=  -O2 -c" "EXTRA_COMPILER_FLAGS=-g -DUSE_AMP=1"
"Compiling usbps"
"Running Make libs in ps7_cortexa9_1/libsrc/xadcps_v2_2/src"
make -C ps7_cortexa9_1/libsrc/xadcps_v2_2/src -s libs  "SHELL=CMD" "COMPILER=arm-xilinx-eabi-gcc" "ARCHIVER=arm-xilinx-eabi-ar" "COMPILER_FLAGS=  -O2 -c" "EXTRA_COMPILER_FLAGS=-g -DUSE_AMP=1"
"Compiling xadcps"
make: Target `all' not remade because of errors.

15:26:59 Build Finished (took 11s.438ms)

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    What version of the SW Speedway are you using? What Vivado version are you using?

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bhfletcher

    Vivado is not used for the SW Speedway. For the SW Speedway I am using the March 7, 2015 version of the pdf training materials.The lab materials list version 2014.4.1. I am using the SDK 2015.4.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bhfletcher

    Vivado is not used for the SW Speedway. For the SW Speedway I am using the March 7, 2015 version of the pdf training materials.The lab materials list version 2014.4.1. I am using the SDK 2015.4.