Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed Power
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 374 subscribers
  • Views 758 views
  • Users 0 members are here
Related

MicroZed Power

raymadigan
raymadigan over 10 years ago

I have a MicroZed and the board usb connector has separated from the board and can no longer provide power :(  Is there any other way to power the board?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Ray,

     

    As discussed in the MicroZed HW Users Guide in section 2.1 you can power the MicroZed via the JX MicroHeaders when plugged into a Carrier Card that supports this, such as the MicroZed FMC Carrier Card or MicroZed IOCC Carrier Card. There is also the option to populate a barrel jack as discussed in section 2.1 of the HW Users Guide as well:

     

    "Populate J4 barrel jack and use a 5V AC/DC supply rated for the projected current demand AND install the capacitors C212, C217, and C218."

     

    The MicroZed HW Users Guide can be downloaded here:

     

    http://zedboard.org/support/documentation/1519

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Ray,

     

    As discussed in the MicroZed HW Users Guide in section 2.1 you can power the MicroZed via the JX MicroHeaders when plugged into a Carrier Card that supports this, such as the MicroZed FMC Carrier Card or MicroZed IOCC Carrier Card. There is also the option to populate a barrel jack as discussed in section 2.1 of the HW Users Guide as well:

     

    "Populate J4 barrel jack and use a 5V AC/DC supply rated for the projected current demand AND install the capacitors C212, C217, and C218."

     

    The MicroZed HW Users Guide can be downloaded here:

     

    http://zedboard.org/support/documentation/1519

     

    -Gary