Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroBlaze with ethernet
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 590 views
  • Users 0 members are here
Related

MicroBlaze with ethernet

waszil
waszil over 8 years ago

Hi!

I have a dual-MicroBlaze design that uses Ethernet (for Spartan-6). Is it possible somehow to implement this existing design into a Zedboard Zynq system? The two MicroBlaze cores should be able to access the Ethernet and the DDR RAM as well. Is it possible?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    It should be possible. Just make sure that the Zedboard has enough logic cells to contain your Spartant 6 design.

    If your question is more along the lines of I wish to use this design that is targerted towards my spartan 6 on a Zedboard withouth an modifications then the answer is most likely no. You will need to recreate your design using Vivado and regenerate your logic targeting the Zedboard and the Zynq 7020 device.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • waszil
    0 waszil over 8 years ago in reply to jafoste4

    Hello,

    I'm OK with re-doing the design in Vivaldo, I'm just not sure if it can be done. What I would like to minimally (as possible) modify is the MicroBlaze firmwares. So you say, it is possible to connect the Microblaze to the onboard Ethernet and RAM? My current design uses SD CARD access also and I would like to skip using the ARM cores as much as possible, but I guess, one ARM core must be used for some FSBL stuff. Is there any tutorial / demo project that is similar to this problem?

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • waszil
    0 waszil over 8 years ago in reply to jafoste4

    Hello,

    I'm OK with re-doing the design in Vivaldo, I'm just not sure if it can be done. What I would like to minimally (as possible) modify is the MicroBlaze firmwares. So you say, it is possible to connect the Microblaze to the onboard Ethernet and RAM? My current design uses SD CARD access also and I would like to skip using the ARM cores as much as possible, but I guess, one ARM core must be used for some FSBL stuff. Is there any tutorial / demo project that is similar to this problem?

    Thanks!