Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Petalinux in the QuadFlash
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 372 subscribers
  • Views 1185 views
  • Users 0 members are here
Related

Petalinux in the QuadFlash

e14 Contributor
e14 Contributor over 11 years ago

Hi Everybody,

I'm new to Xilinx and Petalinux and I'm feeling a little confused about the images i can create with the Petalinux Utilities and which is the way i should download it to the flash in the Microzed 7010.

This is what i have done:

1. Install Petalinux
2. Create a petalinux project based in the 7010 bsp

Now in the .../image/linux/ folder i have a lot of images:

- image.elf
- image.ub
- rootfs.cpio
- rootfs.cpio.gz
- system.dtb
- System.map.lynux
- u-boot.bin
- u-boot.elf
- u-boot.srec
- u-boot-s.bin
- u-boot-s.elf
- u-boot-s.srec
- urootfs.cpio.gz
- vmlinux
- zImage
- zynq_fsbl.elf

My intention is to download and image or images to the quadFlash memory in order to start the linux that I already test in QEMU.

So, would you please guide me in the process to create the images i need to download to the board?

And about the bit-stream image, i also create a project for this specific board and exported the .bit file so i can use it for my system. Is there anything else i need to export to create the entire system images?

Thanks,

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    i followed the tutorial "Booting PicoZed Using QSPI and eMMC v2.1". It's for picozed but it works for microzed too.
    If cat /proc/mtd doesn't work, add thsi to your system-top.dts:
    &qspi {
    flash0: flash@0 {
    compatible = "micron,n25q128a13";
    };
    };

    Thanks Kevin for this post.
    http://zedboard.org/content/unable-read-mtd-picozed-linux

    regards,
    Sebastian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    i followed the tutorial "Booting PicoZed Using QSPI and eMMC v2.1". It's for picozed but it works for microzed too.
    If cat /proc/mtd doesn't work, add thsi to your system-top.dts:
    &qspi {
    flash0: flash@0 {
    compatible = "micron,n25q128a13";
    };
    };

    Thanks Kevin for this post.
    http://zedboard.org/content/unable-read-mtd-picozed-linux

    regards,
    Sebastian