Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ARM processors are slow?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 313 views
  • Users 0 members are here
Related

ARM processors are slow?

e14 Contributor
e14 Contributor over 12 years ago

I have a byte-parsing application that I want to run on the Zynq under Linux. I've bench-marked this on my tired-out Linux web server and can perform a parse there in 4.0 uSec. I've ported this same code to the ZedBoard and found that parse times are about 48 uSecs there, a twelve-fold increase in processing time. Does this seem reasonable? I run the parse 1,000,000 times, so the timings are obvious to me, as I have to wait 48 seconds for the app to complete.

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    I'm not sure there is enough information to guess what is going on. How did you create your hardware platform? If you are using the ones from the Zynq or Linux Intro Speedways, the ARM cpus are running at 667 MHz with the DDR3 running at 533 MHz. Will you tell us a little bit more about what you are doing, or share your project?

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to bhfletcher

    Hi Bryan! I can't share the project, as its technology I want to monetize. I'm running the supplied (on the flash) Linux, and built the ARM executable using the supplied cross-compiler and a -static link. The app itself, after initialization, is nothing but cpu. I ran the last tests with top running, and I can see the app is using an entire core, which is what I would expect.