Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General error detect phy
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 373 subscribers
  • Views 954 views
  • Users 0 members are here
Related

error detect phy

e14 Contributor
e14 Contributor over 9 years ago

Hi!
I have a problem with Lab3 and was wondering if someone could help me please. I keep running in this error in Lab3/ Peripheral Test: "Error detect phy"
the full output when launchig that test is:
---Entering main---
Running ScuGicSelfTestExample() for ps7_scugic_0...
ScuGicSelfTestExample PASSED
ScuGic Interrupt Setup PASSED
Running Interrupt Test for ps7_ethernet_0...
Error detect phy
there is nothing happening afterwards.
i also tested this with the solution to lab 3 and there is the same error message and the exact same behaviour. Could someone please tell me waht is going on? is my board broken or is this another problem?
I'm running vivado2016.2;my board is picozed xc7z015.
Regards,

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Wangy,

    I see your using a PicoZed 7015, which Carrier Card are you using, V1 or V2? I also see you are using Vivado 2016.2, which Tutorial version are you using, 2015.4? If that is the case try downloading the corresponding Vivado Version based on which tutorial you are doing. 

    Also did the other tests work? Such as the Memory Test and Hello World Test? Another question I have for you is are you sure your PicoZed Board is set to JTAG Boot?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hi JFoster,

    Thank you for your answer,

    Yes ,I am using picozed 7015,carrier card is V1 and vivado is 2016.2. Tutorial version is 2015.4,but Memory Test and Hello World are working,only peripheral Test have problems ,when I run as ...,Terminal shows   Running Interrupt Test for ps7_ethernet_0...   Error detect phy.

     I am sure PicoZed Board is set to JTAG Boot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Wangy,

    Start by downloading Vivado/SDK 2015.4 and running through the lab with that version. We specifically designed the Tutorial version 2015.4 to work with Vivado/SDK 2015.4. This would explain why the solutions did not work for you as you were running a 2015.4 version in 2016.2.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 9 years ago

    Wangy,

     

    What is your PicoZed version? Note that Rev C02 and earlier had an Ethernet timing circuit that held the reset too long. You may find that the test passes if you put a delay into the code before you try to exercise the Ethernet.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hello JFoster,

    I am running a 2015.4 .This has also the same problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to bhfletcher

    Hello fletch,

    My picozed version is xc7z015 carries card V1. So how can I put a delay into the code before I try to exercise the Ethernet. 

    I am a newer, thanks for your answer.

     

    wangy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago
    Hello World
    --Starting Memory Test Application--
    NOTE: This application runs with D-Cache disabled.As a result, cacheline request
    s will not be generated
    Testing memory region: ps7_ddr_0
        Memory Controller: ps7_ddr
             Base Address: 0x00100000
                     Size: 0x3ff00000 bytes 
              32-bit test: PASSED!
              16-bit test: PASSED!
               8-bit test: PASSED!
    Testing memory region: ps7_ram_1
        Memory Controller: ps7_ram
             Base Address: 0xffff0000
                     Size: 0x0000fe00 bytes 
              32-bit test: PASSED!
              16-bit test: PASSED!
               8-bit test: PASSED!
    --Memory Test Application Complete--
    ---Entering main---
     
     Running ScuGicSelfTestExample() for ps7_scugic_0...
    ScuGicSelfTestExample PASSED
    ScuGic Interrupt Setup PASSED
     
    Running GpioInputExample() for axi_gpio_1...
    GpioInputExample PASSED. Read data:0x3
     
     Running DcfgSelfTestExample() for ps7_dev_cfg_0...
    DcfgSelfTestExample PASSED
     
     Running XDmaPs_Example_W_Intr() for ps7_dma_s...
    Test round 0
    XDmaPs_Example_W_Intr PASSED
     
     Running Interrupt Test  for ps7_ethernet_0...
    Error detect phy
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hello JFoster

      My teacher told me just that my board is used with MII(100M),rather than GMII(1000M).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Hello fletch

      My teacher told me just that my board is used with MII(100M),rather than GMII(1000M).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Wangy,

    I just went through the design myself with a PicoZed 7015 and FMC Carrier Card V1, and all worked properly. My suggestion would be to download Vivado/SDK 2015.4 and then run the Peripheral Test from the 2015.4 Solution. This will help to determine if you have an issue with your Hardware Design or an issue with your PicoZed SOM.

    --Josh