Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General USB UART doesn't enumerate
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 434 views
  • Users 0 members are here
Related

USB UART doesn't enumerate

e14 Contributor
e14 Contributor over 12 years ago

I've just received my ZedBoard, and have followed the 'getting started' instructions.

The Cypress USB-to-UART driver installed correctly, but most of the time I do not get an enumerated COM port. Very occasionally, after multiple power cycles, I can eventually get it to enumerate and give me COM4, after which I can successfully use Tera Term to talk to the board.

Does anyone have a suggestion as to what the problem is here? I can only imagine that this is a faulty board. I've tried on two different PCs, and have the same behaviour.

The board always appears to boot, and I get the 'Digilent' logo appearing on the LCD display, but most of the time the USB UART does not enumerate and give me a COM port.

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    If you leave the terminal open to a previous successful open COM, then it will block that COM. If you can, please find a different cable and try it because it could be a bad cable. Otherwise, I think you are looking at a faulty board, and you would need to request an RMA from wherever you bought the board.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks Bryan, it turned out to be a bad cable in the end. Swapped the cable, and all seems to be working fine.