Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Ubuntu SAMBA mounting fail
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 438 views
  • Users 0 members are here
Related

Ubuntu SAMBA mounting fail

e14 Contributor
e14 Contributor over 12 years ago

Hi all,
I've followed the Ubuntu Desktop Linux tutorial (http://www.zedboard.org/sites/default/files/design/Ubuntu_on_Zedboard_Tutorial_v14.4_02.pdf) and I've successfully created my Ubuntu sdcard image.

Now I have a big problem: I need to mount a remote folder and I'm not able to do it, neither using cifs/samba neither using nfs

When I run the following line

sudo mount -t cifs //192.168.1.200/REMOTE_FOLDER LOCAL_FOLDER/ -o user=username,pass=password


(I've changed the names, but when I run it they are the correct ones, and the same string works on my ubuntu pc)
This is the answer.

mount error: cifs filesystem not supported by the system
mount error(19): No such device
Refer to the mount.cifs(8) manual page (e.g. man mount.cifs)

The same thing happens when I try to do it with nfs.

A suspicious thing is that when I try to understand if cifs or nfs are installed with modprobe

sudo modprobe cifs

this is the answer

FATAL: Could not load /lib/modules/3.10.0-ga863211/modules.dep: No such file or directory

And I realized that in /lib/modules is empty.

Another thing is that, if explore the folder using Nautilus grafical interface (Go->Location and then smb://192.168...etc) I see it.

So, I can explore it with Nautilus, but I can't mount it.

I have a lot of other problems, so I think that I'm missing something important. Any advice will be appreciated.

Thanks,

Andrea

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The error message is clear: cifs support is not compiled into the kernel, rebuild it with cifs support (File Systems/Network File Systems/Cifs support).
    Nautilus uses a userspace program to access smb drives.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The error message is clear: cifs support is not compiled into the kernel, rebuild it with cifs support (File Systems/Network File Systems/Cifs support).
    Nautilus uses a userspace program to access smb drives.