Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General LWIP Echo Server on a MicroZed board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 531 views
  • Users 0 members are here
Related

LWIP Echo Server on a MicroZed board

e14 Contributor
e14 Contributor over 11 years ago

Hi Folks,

I am trying to run the LWIP echo server on my MicroZed development board.  I am using the example project that came with the software.  It is unmodified except that I changed the ip address and port.  I compiled, downloaded and ran the code.  The console output appears to indicate that it is running correctly but, when I send TCP packets to it, they do not echo back. 

I suspect that the code is good but that I may not be using the board correctly.  I can set the jumpers to run as linux from the QSPI device.  That seems to work as a linux device but I don't know how to run my code from there.  I can also set the jumpers to use JTAG.  When I do that, I can download and run programs but they do not seem to access the ethernet interface. 

How can I run from JTAG and use the ethernet interface for my applications at the same time?  Also, when the application is running correctly, how can I set it up to be non-volatile so that it will not need to be downloaded?

Thank you and best regards, MRL

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Could you give us a little more information.

     

    What example project are you referring to? Where did you get/download it? Does it target the MicroZed board?

     

    Are you trying to run an application under Linux or a 'bare metal' standalone application?

     

    What version of the Xilinx tools are you using? What does the network connection between your MicroZed board and your host PC look like?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Could you give us a little more information.

     

    What example project are you referring to? Where did you get/download it? Does it target the MicroZed board?

     

    Are you trying to run an application under Linux or a 'bare metal' standalone application?

     

    What version of the Xilinx tools are you using? What does the network connection between your MicroZed board and your host PC look like?

     

    -Gary