Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General arm-linux-gcc: command not found
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 1009 views
  • Users 0 members are here
Related

arm-linux-gcc: command not found

e14 Contributor
e14 Contributor over 11 years ago

Hi,
i tried to build u-boot and get this error message:
arm-linux-gcc: command not found

I use Centos7 64bit.
I installed gcc-arm-linux-gnu-4.8.1-5.2.el7.1.x86_64

What can i do to get this working?
I only found tutorials and post about ubuntu but its not working on centos.

I hope you can help me.
Thanks
Max

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The packages required may be different for Ubuntu and Centos. You can look at the steps in Xilinx UG976 and UG983 as an example:

     

    http://www.xilinx.com/support/documentation/sw_manuals/petalinux2014_2/ug976-petalinux-installation.pdf

     

    http://www.xilinx.com/support/documentation/sw_manuals/petalinux2014_2/ug983-petalinux-firmware-upgrade.pdf

     

    You could also look at the Petalinux Software Reference Design for the Mini-ITX board which uses a Centos VM as well:

    http://zedboard.org/support/design/2056/17

     

    If you are using Vivado 2014.2 there is an Answer Record regarding using Virtual Machines you may want to look at as well:

     

    http://www.xilinx.com/support/answers/60485.html

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    i fixed it :)
    i forgot to add the arm-xilinx-linux-gnueabi location to the environment path.

    thanks for you help