Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Where to dowload u-boot Speedway patch and other similar files?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 511 views
  • Users 0 members are here
Related

Where to dowload u-boot Speedway patch and other similar files?

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I am trying to go through all the labs dedicated to Linux boot on Zedboard. In lab 1_2 (v05) experiment 2, you're supposed to apply a patch that is found in the Windows directory C:SpeedwayFall_12Zynq_Linuxlab1_2. Where can I download this patch and, more generally, all the material that is expected to be on the Windows workstations of Speedway classes?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    When you download the zip file for the Labs the patch you are looking for is in the lab1_2 folder in the Zynq_Linux directory. If you unzip the files into the C:Speedway\Fall_12 directory it should be there as indicated.

     

    This training was done with the 14.2 version of the Xilinx tools. If you use a current version of the Xilinx tools to implement these labs you will have to make some adjustments.  If you take a look at the modifications to the labs detailed in the  Open Source Linux USB Host Tutorial, version 14.5 here: http://www.zedboard.org/design/1521/11

    it will get you part of the way. I don't think the script to update the devicetree.dtb will work, you will probably need to make the required modifications by hand. Of course you don't need to do the final steps for the USB Host stuff.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    When you download the zip file for the Labs the patch you are looking for is in the lab1_2 folder in the Zynq_Linux directory. If you unzip the files into the C:Speedway\Fall_12 directory it should be there as indicated.

     

    This training was done with the 14.2 version of the Xilinx tools. If you use a current version of the Xilinx tools to implement these labs you will have to make some adjustments.  If you take a look at the modifications to the labs detailed in the  Open Source Linux USB Host Tutorial, version 14.5 here: http://www.zedboard.org/design/1521/11

    it will get you part of the way. I don't think the script to update the devicetree.dtb will work, you will probably need to make the required modifications by hand. Of course you don't need to do the final steps for the USB Host stuff.

     

    -Gary