Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Getting Started Guide, Windows requirement?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 550 views
  • Users 0 members are here
Related

Getting Started Guide, Windows requirement?

e14 Contributor
e14 Contributor over 14 years ago

I took a quick look at the Getting Started Guide document. 

Page 11 says "The host PC must run Windows (XP/Vista/7)".  If that is truly the case then I won't be purchasing the zedboard.  I am pretty sure that the zedboard should run with a linux host PC, please let me know about this.

Perhaps the guide could be changed to say something like "the following instructions apply for a host PC that runs Windows (XP/Vista/7).  Instructions for operating the zedboard with a linux host PC can be accessed here <zedboard linux host PC web page>.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    piller,

    The User Guide is just describing the configuration that is known to work with the Zedboard.  Since the Cypress device on the board enumerates as a COM device when plugged in, the drivers should load without a problem under Linux.

    As for the terminal program, rather than TeraTerm you can use minicom (or any other terminal software that you prefer) to get the same result.

    You can run this command:

    $ dmesg | grep tty

    after you pug in the USB cable that is plugged into the UART USB port on the Zedboard to display the stty device it was mapped to.

    The command would then be:

    $ minicom -s

    Then you want to set up your configuration to the correct serial port, for me it was /dev/ttyS2.  And the remaining settings are 115200 8N1. (that is a speed of 115200 bps, 8 data bits, no flow control, and 1 stop bit).

    Hope that helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    piller,

    The User Guide is just describing the configuration that is known to work with the Zedboard.  Since the Cypress device on the board enumerates as a COM device when plugged in, the drivers should load without a problem under Linux.

    As for the terminal program, rather than TeraTerm you can use minicom (or any other terminal software that you prefer) to get the same result.

    You can run this command:

    $ dmesg | grep tty

    after you pug in the USB cable that is plugged into the UART USB port on the Zedboard to display the stty device it was mapped to.

    The command would then be:

    $ minicom -s

    Then you want to set up your configuration to the correct serial port, for me it was /dev/ttyS2.  And the remaining settings are 115200 8N1. (that is a speed of 115200 bps, 8 data bits, no flow control, and 1 stop bit).

    Hope that helps!