Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Using Linaro Linux and programming PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 373 subscribers
  • Views 1334 views
  • Users 0 members are here
Related

Using Linaro Linux and programming PL

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I am relatively new to FPGA programming and I have a really simple question.

I have managed to boot Linaro UBUNTU on ZEDBoard from the SD card using the following guide:

http://svenand.blogdrive.com/archive/199.html#.VGvS3qEZW1E

It looks great! However, I cannot understand how I can have the PL programmed AND at the same time have Linaro UBUNTU running. For example, how can I program the PL side while booting AND run ubuntu on the PS side.

My target: what I want to do is process a signal on the PL side that is fed into the PL logic from a PMOD. Then the PL processes the signal and feeds it to the PS (running ubuntu). Then ubuntu decodes the signal and processes it (example: a video signal that is decoded by gstreamer on the PS and viewed on the monitor).

Thank you in advance,

Nick

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Again!

    I will try to answer my questions:

    1) According to :
    'Ubuntu Desktop Linux reference design'
    http://zedboard.org/sites/default/files/design/ZedBoard_Ubuntu_FAT_v2013_4.zip

    I have to use Xilinx SDK in order to create the Boot image which will incorporate:
    a) The First Stage Bool Loader
    b) PL bit stream
    c) U-BOOT
    The output would be a data structure called the Boot Image Format (BIF).

    2)I believe the answer to my 2nd question regarding the design is:

    HDMI Bare Metal Reference Design Using ADV7511 and ADI IP
    http://zedboard.org/sites/default/files/design/ZedBoard_HDMI_Ref_Des_2013_4.zip

    but I have NOT tried it yet.

    The (final?) question still remains whether the 'bit inversion' step is necessary.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Again!

    I will try to answer my questions:

    1) According to :
    'Ubuntu Desktop Linux reference design'
    http://zedboard.org/sites/default/files/design/ZedBoard_Ubuntu_FAT_v2013_4.zip

    I have to use Xilinx SDK in order to create the Boot image which will incorporate:
    a) The First Stage Bool Loader
    b) PL bit stream
    c) U-BOOT
    The output would be a data structure called the Boot Image Format (BIF).

    2)I believe the answer to my 2nd question regarding the design is:

    HDMI Bare Metal Reference Design Using ADV7511 and ADI IP
    http://zedboard.org/sites/default/files/design/ZedBoard_HDMI_Ref_Des_2013_4.zip

    but I have NOT tried it yet.

    The (final?) question still remains whether the 'bit inversion' step is necessary.