Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Using Linaro Linux and programming PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 373 subscribers
  • Views 1332 views
  • Users 0 members are here
Related

Using Linaro Linux and programming PL

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I am relatively new to FPGA programming and I have a really simple question.

I have managed to boot Linaro UBUNTU on ZEDBoard from the SD card using the following guide:

http://svenand.blogdrive.com/archive/199.html#.VGvS3qEZW1E

It looks great! However, I cannot understand how I can have the PL programmed AND at the same time have Linaro UBUNTU running. For example, how can I program the PL side while booting AND run ubuntu on the PS side.

My target: what I want to do is process a signal on the PL side that is fed into the PL logic from a PMOD. Then the PL processes the signal and feeds it to the PS (running ubuntu). Then ubuntu decodes the signal and processes it (example: a video signal that is decoded by gstreamer on the PS and viewed on the monitor).

Thank you in advance,

Nick

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You do not need to perform any 'bit inversion step' if you plan to use the SDK to generate a Boot image that includes the PL bit stream to be loaded at boot time.

     

    If you want to prepare a PL bit file to load after Linux has booted (cat the bit file to /dev/xdevcfg) you will need to perform the file conversion to accomodate file differences.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You do not need to perform any 'bit inversion step' if you plan to use the SDK to generate a Boot image that includes the PL bit stream to be loaded at boot time.

     

    If you want to prepare a PL bit file to load after Linux has booted (cat the bit file to /dev/xdevcfg) you will need to perform the file conversion to accomodate file differences.

     

    -Gary