Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General U-boot won't boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 373 subscribers
  • Views 3525 views
  • Users 0 members are here
Related

U-boot won't boot

e14 Contributor
e14 Contributor over 12 years ago

I am not able to get U-boot up and running on my MicroZed board. I tried to have it loaded by Xilinx first stage bootloader (FSBL) and I have tried starting it from the XMD shell over JTAG.


I do not get any output from U-boot in the shell (connector J17 - USB UART).


When loaded by FSBL, it seems that U-boot crashes. Some times FSBL is restarted a couple of times (its output to the UART is repeated). Some times the FSBL exception handlers is invoked after handoff:


In FsblHookBeforeHandoff function                                              
SUCCESSFUL_HANDOFF                                                             
FSBL Status = 0x1                                                              
DATA_ABORT_HANDLER                                                             
FSBL Status = 0xA304


I have build FSBL using Release 14.6 Build SDK_P.68d and with the flags "-DFSBL_DEBUG -DFSBL_DEBUG_INFO". I have also tried without these flags.


I have made the U-boot image using:


$ git clone git://git.xilinx.com/u-boot-xlnx.git
$ cd u-boot-xlnx
$ PATH=$PATH:/opt/Xilinx/SDK/2013.2/gnu/arm/lin/bin
$ export CROSS_COMPILE=arm-xilinx-linux-gnueabi-
$ make zynq_zed_config && make


The boot.bin file was created using:


$ cat zed_boot.bif
zed_boot_image:
{
t[bootloader]zed_fsbl.elf
tzed_u-boot.elf
}
$ bootgen -image zed_boot.bif -o boot.bin -w on


This is the output I get in the shell:


Xilinx First Stage Boot Loader
Release 14.6/2013.2     Sep 27 2013-09:39:00
Devcfg driver initialized
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD Init Done
Flash Base Address: 0xE0100000
Reboot status register: 0x60600000
Multiboot Register: 0x0000C000
Image Start Address: 0x00000000
Partition Header Offset:0x00000980
Partition Count: 2
Partition Number: 1
Header Dump
Image Word Len: 0x00010174
Data Word Len: 0x00010174
Partition Word Len:0x00010174
Load Addr: 0x04000000
Exec Addr: 0x04000000
Partition Start: 0x000062A0
Partition Attr: 0x00000010
Partition Checksum Offset: 0x00000000
Section Count: 0x00000001
Checksum: 0xF7FC96A2
Application
Handoff Address: 0x04000000
In FsblHookBeforeHandoff function
SUCCESSFUL_HANDOFF
FSBL Status = 0x1


When starting U-boot from the XMD shell, I do the following, which produces no output in the J17 USB UART shell:


$ /opt/Xilinx/14.6/ISE_DS/EDK/bin/lin/xmd
XMD% connect arm hw
XMD% source /opt/Xilinx/14.6/ISE_DS/EDK/sw/lib/hwplatform_templates/zed_hw_platform/ps7_init.tcl
XMD% ps7_init
XMD% dow zed_u-boot.elf
XMD% con


I read a post stating the Xilinx U-boot image for the ZC702 board could be used on the MicroZed board to. I tried that with the same result.


Using the XMD shell I read the memory at location 0x04000000:
XMD% mrd 0x04000000 30
4000000:   00000000
4000004:   E59FF014
4000008:   E59FF014
400000C:   E59FF014
4000010:   E59FF014
4000014:   E59FF014
4000018:   E59F7BDD
400001C:   E59FDDC8
4000020:   04F1E934
4000024:   04007D23
4000028:   0400B956
400002C:   0400EDFB
4000030:   04007F6B
4000034:   0400DFAF
4000038:   0400F357
400003C:   1234D563


It seems to be the same image as zed_u-boot.elf from 0x8000 bytes into the zed_u-boot.elf. I expect this is because the elf header was removed.


I have run out of ideas of what to try, so any hints will be appreciated.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Are you using MizroZed or Zedboard? They have different hardware, and so (slightly, but still) different MIO pinout and different FSBL (if you are using Xilinx tools).
    If you use MicroZed board, you may try alternative software, configuration files so far exist for MicroZed only. For debugging it allows you to control LED and UART output during the initial stages of booting, before U-boot prompt,
    http://sourceforge.net/p/elphel/ezynq/ - standalone version
    http://sourceforge.net/p/elphel/meta-ezynq - OpenEmbedded meta

    Andrey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I'm using MicroZed.

    1) Are you saying that the Xilinx U-boot repository does not have support for the MicroZed board?
    Quite annoying Avnet hasn't pushed their MicroZed files upstream yet (a working U-boot is shipped with the board in its NOR flash)...

    2) Do you know whether there are any issues using "zed_hw_platform" in the Xilinx SDK for making an FSBL for MicroZed?
    Enabling debug in the FSBL, it seems to work fine, but I don't know if there are something it might not have configured or configured wrong.

    3) Is there some official MicroZed tutorial or guide I have overlooked, which produce a working version of U-boot for MicroZed?

    I tried to build from you reference (standalone version), but the build fails:
    make[1]: Entering directory `elphel-ezynq/u-boot-xlnx/arch/arm/cpu/armv7/zynq'
    make[1]: *** No rule to make target `.depend', needed by `all'.  Stop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Kian,

    can you please post here or (to save bandwidth) email it to me at andrey_at_elphel.com the full output install_uboot.sh and makeuboot? I just tried in on a fresh computer w/o any problems.

    1) When we got MicroZed in August, there was none.
    2) Zedboard and Microzed have different connections, but we were able to make a working image with Xilinx tools, carefully entering data from the MicroZed documentation. MIO pins are different for 2 boards
    3) Circuit diagram+documentation that are available for the board are sufficient to produce a working version. I can not send you our files produceds by Xilinx tools because Xilinx license does not allow such distribution.

    Andrey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Kian,

    can you please post here or (to save bandwidth) email it to me at andrey_at_elphel.com the full output install_uboot.sh and makeuboot? I just tried in on a fresh computer w/o any problems.

    1) When we got MicroZed in August, there was none.
    2) Zedboard and Microzed have different connections, but we were able to make a working image with Xilinx tools, carefully entering data from the MicroZed documentation. MIO pins are different for 2 boards
    3) Circuit diagram+documentation that are available for the board are sufficient to produce a working version. I can not send you our files produceds by Xilinx tools because Xilinx license does not allow such distribution.

    Andrey