Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General U-boot won't boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 373 subscribers
  • Views 3519 views
  • Users 0 members are here
Related

U-boot won't boot

e14 Contributor
e14 Contributor over 12 years ago

I am not able to get U-boot up and running on my MicroZed board. I tried to have it loaded by Xilinx first stage bootloader (FSBL) and I have tried starting it from the XMD shell over JTAG.


I do not get any output from U-boot in the shell (connector J17 - USB UART).


When loaded by FSBL, it seems that U-boot crashes. Some times FSBL is restarted a couple of times (its output to the UART is repeated). Some times the FSBL exception handlers is invoked after handoff:


In FsblHookBeforeHandoff function                                              
SUCCESSFUL_HANDOFF                                                             
FSBL Status = 0x1                                                              
DATA_ABORT_HANDLER                                                             
FSBL Status = 0xA304


I have build FSBL using Release 14.6 Build SDK_P.68d and with the flags "-DFSBL_DEBUG -DFSBL_DEBUG_INFO". I have also tried without these flags.


I have made the U-boot image using:


$ git clone git://git.xilinx.com/u-boot-xlnx.git
$ cd u-boot-xlnx
$ PATH=$PATH:/opt/Xilinx/SDK/2013.2/gnu/arm/lin/bin
$ export CROSS_COMPILE=arm-xilinx-linux-gnueabi-
$ make zynq_zed_config && make


The boot.bin file was created using:


$ cat zed_boot.bif
zed_boot_image:
{
t[bootloader]zed_fsbl.elf
tzed_u-boot.elf
}
$ bootgen -image zed_boot.bif -o boot.bin -w on


This is the output I get in the shell:


Xilinx First Stage Boot Loader
Release 14.6/2013.2     Sep 27 2013-09:39:00
Devcfg driver initialized
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD Init Done
Flash Base Address: 0xE0100000
Reboot status register: 0x60600000
Multiboot Register: 0x0000C000
Image Start Address: 0x00000000
Partition Header Offset:0x00000980
Partition Count: 2
Partition Number: 1
Header Dump
Image Word Len: 0x00010174
Data Word Len: 0x00010174
Partition Word Len:0x00010174
Load Addr: 0x04000000
Exec Addr: 0x04000000
Partition Start: 0x000062A0
Partition Attr: 0x00000010
Partition Checksum Offset: 0x00000000
Section Count: 0x00000001
Checksum: 0xF7FC96A2
Application
Handoff Address: 0x04000000
In FsblHookBeforeHandoff function
SUCCESSFUL_HANDOFF
FSBL Status = 0x1


When starting U-boot from the XMD shell, I do the following, which produces no output in the J17 USB UART shell:


$ /opt/Xilinx/14.6/ISE_DS/EDK/bin/lin/xmd
XMD% connect arm hw
XMD% source /opt/Xilinx/14.6/ISE_DS/EDK/sw/lib/hwplatform_templates/zed_hw_platform/ps7_init.tcl
XMD% ps7_init
XMD% dow zed_u-boot.elf
XMD% con


I read a post stating the Xilinx U-boot image for the ZC702 board could be used on the MicroZed board to. I tried that with the same result.


Using the XMD shell I read the memory at location 0x04000000:
XMD% mrd 0x04000000 30
4000000:   00000000
4000004:   E59FF014
4000008:   E59FF014
400000C:   E59FF014
4000010:   E59FF014
4000014:   E59FF014
4000018:   E59F7BDD
400001C:   E59FDDC8
4000020:   04F1E934
4000024:   04007D23
4000028:   0400B956
400002C:   0400EDFB
4000030:   04007F6B
4000034:   0400DFAF
4000038:   0400F357
400003C:   1234D563


It seems to be the same image as zed_u-boot.elf from 0x8000 bytes into the zed_u-boot.elf. I expect this is because the elf header was removed.


I have run out of ideas of what to try, so any hints will be appreciated.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 12 years ago

    Hi kkaras,

    After looking into this further, I found that the U-Boot binary which is shipping on MicroZed and distributed in the "MicroZed Linux microSD Card Image Archive 10.Aug.13" found on this page: http://www.microzed.org/documentation/1519 is publicly available from Xilinx from their GIT repository located here:

    https://github.com/Xilinx/u-boot-xlnx

    That binary provided in the MicroZed Linux microSD Archive was built directly from the xilinx-v14.5 release tag on that repository using the zynq_zed configuration since it is part of the Zed family of boards and is very similar to ZedBoard hardware configuration as far as U-Boot is concerned.

    The dirty tag on the build is from the result of modification to the one of the configuration files for the default U-Boot environment.  This modification was made to support the MTD partitioning that was selected and to allow the second stage boot loader (U-Boot) to perform the PL configuration rather than have this task performed by the FSBL.

    In particular, these extra environment variables are used to support these features of MicroZed.

    #define CONFIG_EXTRA_ENV_SETTINGSt
    t"ethaddr=00:0a:35:00:01:220"t
    t"kernel_image=uImage0"t
    t"ramdisk_image=uramdisk.image.gz0"t
    t"devicetree_image=devicetree.dtb0"t
    t"bitstream_image=system.bit.bin0"t
    t"bitstream_size=0x3DBAFC0"t
    t"loadbit_addr=0x1000000"t
    t"kernel_size=0x5000000"t
    t"devicetree_size=0x200000"t
    t"ramdisk_size=0x5E00000"t
    t"fdt_high=0x200000000"t
    t"initrd_high=0x200000000"t
    t"mmc_loadbit_fat=echo Loading bitstream from SD/MMC/eMMC to RAM.. && "
    tt"mmcinfo && "
    tt"fatload mmc 0 ${loadbit_addr} ${bitstream_image} && "
    tt"fpga load 0 ${loadbit_addr} ${filesize}0"
    t"norboot=echo Copying Linux from NOR flash to RAM... && "
    tt"cp 0xE2100000 0x3000000 ${kernel_size} && "
    tt"cp 0xE2600000 0x2A00000 ${devicetree_size} && "
    tt"echo Copying ramdisk... && "
    tt"cp 0xE2620000 0x2000000 ${ramdisk_size} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"qspiboot=echo Copying Linux from QSPI flash to RAM... && "
    tt"sf probe 0 0 0 && "
    tt"sf read ${loadbit_addr} 0xC00000 ${bitstream_size} && "
    tt"mw 0xF8007080 0x30800100 0x4 && "
    tt"fpga load 0 ${loadbit_addr} ${bitstream_size} && "
    tt"sf read 0x3000000 0x100000 ${kernel_size} && "
    tt"sf read 0x2A00000 0x600000 ${devicetree_size} && "
    tt"echo Copying ramdisk... && "
    tt"sf read 0x2000000 0x620000 ${ramdisk_size} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"sdboot=echo Copying Linux from SD to RAM... && "
    tt"mmcinfo && "
    tt"run mmc_loadbit_fat && "
    tt"fatload mmc 0 0x3000000 ${kernel_image} && "
    tt"fatload mmc 0 0x2A00000 ${devicetree_image} && "
    tt"fatload mmc 0 0x2000000 ${ramdisk_image} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"nandboot=echo Copying Linux from NAND flash to RAM... && "
    tt"nand read 0x3000000 0x100000 ${kernel_size} && "
    tt"nand read 0x2A00000 0x600000 ${devicetree_size} && "
    tt"echo Copying ramdisk... && "
    tt"nand read 0x2000000 0x620000 ${ramdisk_size} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"jtagboot=echo TFTPing Linux to RAM... && "
    tt"tftp 0x3000000 ${kernel_image} && "
    tt"tftp 0x2A00000 ${devicetree_image} && "
    tt"tftp 0x2000000 ${ramdisk_image} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"

    I apologize that these details have not been placed into a tutorial yet.  I plan to do this shortly or replace these MicroZed binaries with a newer release tag which can be supported longer (with tutorials also).

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 12 years ago

    Hi kkaras,

    After looking into this further, I found that the U-Boot binary which is shipping on MicroZed and distributed in the "MicroZed Linux microSD Card Image Archive 10.Aug.13" found on this page: http://www.microzed.org/documentation/1519 is publicly available from Xilinx from their GIT repository located here:

    https://github.com/Xilinx/u-boot-xlnx

    That binary provided in the MicroZed Linux microSD Archive was built directly from the xilinx-v14.5 release tag on that repository using the zynq_zed configuration since it is part of the Zed family of boards and is very similar to ZedBoard hardware configuration as far as U-Boot is concerned.

    The dirty tag on the build is from the result of modification to the one of the configuration files for the default U-Boot environment.  This modification was made to support the MTD partitioning that was selected and to allow the second stage boot loader (U-Boot) to perform the PL configuration rather than have this task performed by the FSBL.

    In particular, these extra environment variables are used to support these features of MicroZed.

    #define CONFIG_EXTRA_ENV_SETTINGSt
    t"ethaddr=00:0a:35:00:01:220"t
    t"kernel_image=uImage0"t
    t"ramdisk_image=uramdisk.image.gz0"t
    t"devicetree_image=devicetree.dtb0"t
    t"bitstream_image=system.bit.bin0"t
    t"bitstream_size=0x3DBAFC0"t
    t"loadbit_addr=0x1000000"t
    t"kernel_size=0x5000000"t
    t"devicetree_size=0x200000"t
    t"ramdisk_size=0x5E00000"t
    t"fdt_high=0x200000000"t
    t"initrd_high=0x200000000"t
    t"mmc_loadbit_fat=echo Loading bitstream from SD/MMC/eMMC to RAM.. && "
    tt"mmcinfo && "
    tt"fatload mmc 0 ${loadbit_addr} ${bitstream_image} && "
    tt"fpga load 0 ${loadbit_addr} ${filesize}0"
    t"norboot=echo Copying Linux from NOR flash to RAM... && "
    tt"cp 0xE2100000 0x3000000 ${kernel_size} && "
    tt"cp 0xE2600000 0x2A00000 ${devicetree_size} && "
    tt"echo Copying ramdisk... && "
    tt"cp 0xE2620000 0x2000000 ${ramdisk_size} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"qspiboot=echo Copying Linux from QSPI flash to RAM... && "
    tt"sf probe 0 0 0 && "
    tt"sf read ${loadbit_addr} 0xC00000 ${bitstream_size} && "
    tt"mw 0xF8007080 0x30800100 0x4 && "
    tt"fpga load 0 ${loadbit_addr} ${bitstream_size} && "
    tt"sf read 0x3000000 0x100000 ${kernel_size} && "
    tt"sf read 0x2A00000 0x600000 ${devicetree_size} && "
    tt"echo Copying ramdisk... && "
    tt"sf read 0x2000000 0x620000 ${ramdisk_size} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"sdboot=echo Copying Linux from SD to RAM... && "
    tt"mmcinfo && "
    tt"run mmc_loadbit_fat && "
    tt"fatload mmc 0 0x3000000 ${kernel_image} && "
    tt"fatload mmc 0 0x2A00000 ${devicetree_image} && "
    tt"fatload mmc 0 0x2000000 ${ramdisk_image} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"nandboot=echo Copying Linux from NAND flash to RAM... && "
    tt"nand read 0x3000000 0x100000 ${kernel_size} && "
    tt"nand read 0x2A00000 0x600000 ${devicetree_size} && "
    tt"echo Copying ramdisk... && "
    tt"nand read 0x2000000 0x620000 ${ramdisk_size} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"
    t"jtagboot=echo TFTPing Linux to RAM... && "
    tt"tftp 0x3000000 ${kernel_image} && "
    tt"tftp 0x2A00000 ${devicetree_image} && "
    tt"tftp 0x2000000 ${ramdisk_image} && "
    tt"bootm 0x3000000 0x2000000 0x2A000000"

    I apologize that these details have not been placed into a tutorial yet.  I plan to do this shortly or replace these MicroZed binaries with a newer release tag which can be supported longer (with tutorials also).

    Regards,

    -Kevin