Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General XAPP1078
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 492 views
  • Users 0 members are here
Related

XAPP1078

e14 Contributor
e14 Contributor over 12 years ago

I downloaded the ZedBoard version of the XAPP1078 reference design and copied the generated files to a SD Card. CPU0 runs Linux fine, but CPU1's bare-metal application does not. I have to connect XMD and send  'con 0x18000000' to get CPU1 to run. The FSBL copies the .elf file into memory okay, but something goes wrong after that. There is a Xilinx wiki page for XAPP1078 that indicates the Xilinx ZC706 board has version 2.0 silicon with a different ROM bootloader requiring changes for the reference design to work. Could this be my problem as well? How do I know which chip version is running on the ZedBoard?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Rev D ZedBoard has the newer, production silicon. A Rev C. ZedBoard has the earlier ES silicon.

     

    You could also read the MCTRL register (see UG585, the Zynq Technical Reference Manual for bit definitions) by launching an XMD console in the SDK with the JTAG cable connected and connect to the ARM by entering "connect arm hw" at the XMD% prompt.

     

    Then enter mrd 0xf8007080 at the next XMD% prompt to read the MCTRL register at 0xF8007080.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Rev D ZedBoard has the newer, production silicon. A Rev C. ZedBoard has the earlier ES silicon.

     

    You could also read the MCTRL register (see UG585, the Zynq Technical Reference Manual for bit definitions) by launching an XMD console in the SDK with the JTAG cable connected and connect to the ARM by entering "connect arm hw" at the XMD% prompt.

     

    Then enter mrd 0xf8007080 at the next XMD% prompt to read the MCTRL register at 0xF8007080.

     

    -Gary