Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General PlanAHead and VHDL-Verilog design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 372 subscribers
  • Views 848 views
  • Users 0 members are here
Related

PlanAHead and VHDL-Verilog design

e14 Contributor
e14 Contributor over 12 years ago

A simple question

what is the best way to design and debugg some vhd file when you are creating and working on a project from planAhead - xps?

i got used to creating my stuff with these two - they are really great once we have gone through the tutorial. And i start creating more complex projects which involve writing my vhd code.
by now i used to write it by hand, mostly modifying "user_logic.vhd" but now i would like to create different level of implemantations and i need syntax debugging, and to me, it is not obvious how we are supposed to do so.

At now the only solution i came up with was to create an ise project with my vhd files including user_logic, doing my work, and then copy the result back into my planAhead project.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    thanks for your answer.

    general process using planAhead links us to generate a .bit and different kind of folders, mainly IPCORE where we are supposed to code our own vhdl.

    my personnal vhdl is programmed inside ISE.
    if i generate a .bit inside ISE that is not relevant to me, in the sense that planAhead generates the .bit with all the hardware specifications related to CPU PS7. that .bit wouldnt be the one we upload to the fpga right?

    samely i dont see how you would link a proper ise project including one or many .vhd constrained by one .ucf to a planAhead project ready to be deployed on the zedboard (since planAhead allows us to create a .ucf for our application .ucf which is located to a particular place, which is /project/constr/new/my.ucf )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    thanks for your answer.

    general process using planAhead links us to generate a .bit and different kind of folders, mainly IPCORE where we are supposed to code our own vhdl.

    my personnal vhdl is programmed inside ISE.
    if i generate a .bit inside ISE that is not relevant to me, in the sense that planAhead generates the .bit with all the hardware specifications related to CPU PS7. that .bit wouldnt be the one we upload to the fpga right?

    samely i dont see how you would link a proper ise project including one or many .vhd constrained by one .ucf to a planAhead project ready to be deployed on the zedboard (since planAhead allows us to create a .ucf for our application .ucf which is located to a particular place, which is /project/constr/new/my.ucf )