Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General PlanAHead and VHDL-Verilog design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 372 subscribers
  • Views 847 views
  • Users 0 members are here
Related

PlanAHead and VHDL-Verilog design

e14 Contributor
e14 Contributor over 12 years ago

A simple question

what is the best way to design and debugg some vhd file when you are creating and working on a project from planAhead - xps?

i got used to creating my stuff with these two - they are really great once we have gone through the tutorial. And i start creating more complex projects which involve writing my vhd code.
by now i used to write it by hand, mostly modifying "user_logic.vhd" but now i would like to create different level of implemantations and i need syntax debugging, and to me, it is not obvious how we are supposed to do so.

At now the only solution i came up with was to create an ise project with my vhd files including user_logic, doing my work, and then copy the result back into my planAhead project.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    Dont be messed up with the software varities..

    in ISE you can write your HDL code,synthesize it...You have to only move to planahead while giving the Pin constraints.and .bit can also be generated in ISE itself..

    Also the whole work can be done on planahead as well

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    Dont be messed up with the software varities..

    in ISE you can write your HDL code,synthesize it...You have to only move to planahead while giving the Pin constraints.and .bit can also be generated in ISE itself..

    Also the whole work can be done on planahead as well