Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Differences between ZedBoard and Xilinx Zynq-7000 SoC ZC702 Evaluation Kit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 372 subscribers
  • Views 5355 views
  • Users 0 members are here
Related

Differences between ZedBoard and Xilinx Zynq-7000 SoC ZC702 Evaluation Kit

e14 Contributor
e14 Contributor over 13 years ago

Hello everybody!

What are the main differences between these two development board? ZedBoard costs 395$, while the Evaluation Kit by Xilinx costs 895$ and I can't understand this evident difference.

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago
            

    Xilinx ZC702

      
       

    Avnet/Digilent ZedBoard

      
       

    Price

      
       

    $895

      
       

    $475

      
       

    Xilinx Part        XC7Z020-1CLG484C(ES)

      
       

    √

      
       

    √

      
       

    Configuration
            1) Onboard configuration circuitry
            2) Quad SPI Flash
            3) SD Card
            4) JTAG Connector

      
       


         SMT2
         128Mb
         8 GB
         √

      
       


         SMT2
         256Mb
         4 GB
         √

      
       

    Memory 

       

        1) RAM
             2) Quad SPI Flash
             3) IIC EEPROM

      
       


         DDR3, 1GB, 533MHz
         128Mb
         1KB

      
       


         DDR3, 512MB, 533MHz
         256Mb
         X

      
       

    Communication
             1) Ethernet
             2) USB 2.0 OTG Port
             3) Serial Port (UART2USB)
             4) CAN

      
       


          10/100/1000
         √ (SMSC PHY)
         √ (SiLabs)
         √

      
       


          10/100/1000
         √  (TI PHY)
         √ (Cypress)
         X

      
       

    Expansion Ports
             1) FMC
             2) PMOD Header
             3) AMS Expansion

      
       


         2x LPC
         12 PL I/Os
         √

      
       


         1x LPC
         8 PS I/Os, 32 PL I/Os
         √

      
       

    User I/O
             1) LEDS
             2) Switches
             3) PBs

      
       


         2 PL
         3 PL
         2 PL

      
       


         1 PS, 8 PL
         8 PL
         2 PS, 5 PL

      
       

    Display and Audio

       

        1) HDMI
             2) VGA
             3) OLED
             4) Audio Codec

      
       


         ADV7511
         X
         X
         X

      
       


         ADV7511
         12-bit color (R-divider)
         128x32
         ADAU1761

      
       

    Power

       

        1) Wall adapter
             2) Separate PS/PL rails
             3) Power Monitor

      
       


         12V @ 5A
         √
         All Rails via TI SW

      
       


         12V @ 5A
          X
         12V only

      
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    Some of the Xilinx materials say "1Gb" DDR3.  I believe that this should be 1GB ( http://www.micron.com/parts/dram/ddr3-sdram/mt41j256m8hx-15e )


    Also, the ZC702 comes with a locked seat of "Embedded Edition of the ISE Design Suite" which may be useful.

    Anyone know if that can be used with the ZedBoard?

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago in reply to e14 Contributor

    The ZC702 has 4 components of 2Gb each, which is a total system memory of 1GB.  Any ZC702 documentation referring to its memory capacity as 1Gb is wrong.

     

    Since the ZC702 and ZedBoard share the same Zynq device (7z020), the 7z020-device-locked software will work with ZedBoard.  I believe the Embedded Edition (compared to the ZedBoard included WebPACK/ChipScope) only adds full ISIM capability.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago in reply to e14 Contributor

    The ZC702 has 4 components of 2Gb each, which is a total system memory of 1GB.  Any ZC702 documentation referring to its memory capacity as 1Gb is wrong.

     

    Since the ZC702 and ZedBoard share the same Zynq device (7z020), the 7z020-device-locked software will work with ZedBoard.  I believe the Embedded Edition (compared to the ZedBoard included WebPACK/ChipScope) only adds full ISIM capability.

     

    Bryan