Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Connecting MicroZed to PC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 374 subscribers
  • Views 676 views
  • Users 0 members are here
Related

Connecting MicroZed to PC

100priya
100priya over 8 years ago

Hi. I have earlier done programming of Zedboard but I m a beginner in terms of programming of microzed board. I have a MicroZed breakout carrier card and a MicroZed board. I don't have Jtag / HS3 cable. Can anyone tell me how do i program microzed board for standalone case without using Jtag / HS3 cable? 

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Priya,

    The only other way is to program an SD card image and manually install that into you MicroZed and then boot from the SD card.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • 100priya
    0 100priya over 8 years ago in reply to jafoste4

    Hi Josh.

    Thanks for replying. While I was looking for a solution to the above mentioned problem,  I read somewhere that Ethernet cable can be used to program MicroZed board. Could you please suggest if it is possible to program using Ethernet instead of booting image to SD card?

    -- Priya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 8 years ago

    Priya,

    I am not aware of a boot-over-Ethernet example. However, you could extract the pre-built boot image from the PetaLinux BSP, copy to an SD Card, then boot MicroZed to PetaLinux, then transfer a new image to the MicroZed, then use PetaLinux to erase and copy the QSPI Flash.

    For the $55, it's probably worth the HS3 cable -- http://avnet.me/jtaghs3. Over 100 in stock. For any serious development, the debugging capability is invaluable.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100priya
    0 100priya over 8 years ago in reply to bhfletcher

    Thank you for your suggestion Bryan. I programmed SD card and booted MicroZed board using it and it worked (for a simple application). But I think I will be purchasing HS3 cable.

    --Priya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sophia1987
    0 sophia1987 over 8 years ago in reply to 100priya

    Hi Priya!

    I had the same issue and must say that HS3 cable solved it once and for all. It should work for you as well. I highly recommend not to wait with buying it.

    Good luck!

    Sophia