Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard and Aptina Image Sensor
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 511 views
  • Users 0 members are here
Related

Zedboard and Aptina Image Sensor

e14 Contributor
e14 Contributor over 11 years ago

I would like to use the ZYNQ 7000 SoC for a video camera development but I am completely new to using an SoC or FPGA. I thought that the zedboard might be a good introductory board to learn FPGA design but I am wondering if the zedboard can be interfaced with my image sensor. Our image sensor is an Aptina CMOS image sensor that uses the HiSPi data interface (high-speed serial pixel interface) sub-LVDS. I just want to know if I will run into interfacing issues before purchasing a zedboard.

  • Sign in to reply
  • Cancel
  • albertabeef
    0 albertabeef over 11 years ago

    Mico,

    I encountered the same situation when designing the Toshiba TCM3232PB camera module.

    Although this camera module interfaces to the MicroZed SOM (via the Embedded Vision carrier card), and not the ZedBoard, it is a similar situation to the one you are describing.  In this case, we were constrained to a 2.5V I/O bank, and did not have the option to add on-board termination at the receiver.  We chose to use a LVDS receiver with internal terminateion (TERM = TRUE).

    Please refer to the Toshiba camera module's hardware user guide for a discussion on the compatibility between a sub-LVDS transmitter (image sensor) and the LVDS_25 receiver on the Zynq-7010/7020 device.  Before we built the hardware, we validated compatibility with a HSpice simulation.

       http://zedboard.org/product/toshiba-industrial-1080p60-camera-module

    The hardware is working.

    Regards,

    Mario

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Guys!
      I ask if did you already use OV7725 to Zedboard?