Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Run linux user application automatically after boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 374 subscribers
  • Views 1908 views
  • Users 0 members are here
Related

Run linux user application automatically after boot

e14 Contributor
e14 Contributor over 12 years ago

I have followed the Zynq Concepts, Tools, and Techniques tutorial and have been able to run the linux hello world application on the sd card from the "zynq> " terminal prompt without issue. How would I get this or some other linux user application to run automatically after the zedboard boots up?

-Pat

  • Sign in to reply
  • Cancel

Top Replies

  • zedhed
    zedhed over 12 years ago +1
    Hi psullivan, I am assuming that this is the 2013.2 CTT you are referring to. One option that works well for me during prototyping is to modify your /etc/init.d/rcS file to mount the SD card under say…
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Take a look at this link to stackoverflow on the subject:

     

    http://stackoverflow.com/questions/17024197/run-application-program-after-linux-bootup-on-arm

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 12 years ago

    Hi psullivan,

    I am assuming that this is the 2013.2 CTT you are referring to.

    One option that works well for me during prototyping is to modify your /etc/init.d/rcS file to mount the SD card under say /mnt and call a startup script.  In fact, if you take a look at the following Wiki entry, it contains a Zynq ramdisk image which already has this modification I refer to:

    http://www.wiki.xilinx.com/Build+and+Modify+a+Rootfs

    If you use the are_ramdisk.image.gz image from this wiki page and rename it to overwrite the ramdisk8M.image.gz from the CTT, you can accomplish this rather quickly.

    If you look at /etc/init.d/rcS in this ramdisk image, it will mount your SD card to /mnt and look for an init.sh script there.  If init.sh exists on the SD card, it will run it automatically.  Simply place your own init.sh onto the SD card and have it call the executable that you want to have launched after Linux boots.

    Start with something simple in init.sh like this:

    #!/bin/sh
    echo "Hello ZedBoard"

    And then work your way up from there.

    Regards,

    -Kevin