Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Using TRACE32 debug on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 776 views
  • Users 0 members are here
Related

Using TRACE32 debug on Zedboard

e14 Contributor
e14 Contributor over 10 years ago

Hello!

I am checking what hardware is needed to enable TRACE32 debug on Zedboard.

As per http://www.lauterbach.com/pro/pro_zynq-7000.php?chip=ZYNQ-7000 - two products are needed, LA-3500 powerdebug and LA-7843 JTAG debugger.

LA-7843 description mentions that it "supports 5-pin standard JTAG, cJTAG and Serial Wire Debug Port (0.4 V - 5 V) ". But the Zedboard spec indicates a 14-pin JTAG connector. Are there standard adapters between what LA-7843 expects and what Zedboard provides?

Thanks,
Karthick

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 10 years ago

    Hi Karthick,

    We do offer this adapter boards which adapts from the ARM 20-pin connector found on most debuggers (this was tested using ARM DSTREAM debugger) to the Xilinx 14-pin JTAG connector found on ZedBoard.  There is another 20-pin connector on ZedBoard but that is for access to the XADC functionality only (not JTAG).

    http://www.em.avnet.com/zeddebugadapter

    This small adapter board will adapt the 14-pin PC4 connector on ZedBoard to the ARM-20 connector seen on this page:

    http://www.lauterbach.com/frames.html?pro/pro_zynq-7000.php?chip=ZYNQ-7000

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 10 years ago

    Hi Karthick,

    We do offer this adapter boards which adapts from the ARM 20-pin connector found on most debuggers (this was tested using ARM DSTREAM debugger) to the Xilinx 14-pin JTAG connector found on ZedBoard.  There is another 20-pin connector on ZedBoard but that is for access to the XADC functionality only (not JTAG).

    http://www.em.avnet.com/zeddebugadapter

    This small adapter board will adapt the 14-pin PC4 connector on ZedBoard to the ARM-20 connector seen on this page:

    http://www.lauterbach.com/frames.html?pro/pro_zynq-7000.php?chip=ZYNQ-7000

    Regards,

    -Kevin