Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Need to Build a Large FIFO on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 372 subscribers
  • Views 1076 views
  • Users 0 members are here
Related

Need to Build a Large FIFO on Zedboard

e14 Contributor
e14 Contributor over 12 years ago

I am using the Zedboard and I am in the need of a large FIFO to buffer data in the PL to eventually move the data to the PS. Currently I am trying to populate a 32 bit wide with at least 500000 depth FIFO buffer but there isnt enough resources in the Zedboard. I am wondering what other possible solutions I have?

One thought was creating multiple FIFOs with diefferent resources (distirbuted ram, BRAM, and FIFO36 blocks) then route the data as each one gets filled up. It seems however that the FIFO36 and the BRAM options use similar resources so I still have a problem. When I try to run the distributed RAM option with huge depth IP doesnt seem to get generated when I start synthesis.

Another thought was using an expansion board. Are there any FMC or PMOD expansion boards that I could use to expand on the exisiting logic in the Zed board? Or can I use another zedboard or microzed to expand?

Any other ideas that might be useful?

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 12 years ago

    Hi,

    Have you considered using the AXI bus to just write directly into the DDR memory that is used by the PS?  You can configure the DMA controller to allow this access.  This is done using the AXI GP interfaces.  Then you only need to set an interrupt (AXI ability) to tell the PS when it needs to manipulate the data.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to drozwood90

    Thanks zedman2000, that sounds like the most reasonable solution I've encountered so far. I was also looking into AXI virtual FIFO but it looks like more than I need. Nevertheless, with the DMA solution that you mentioned it seems like the DMA controller hooks up to AXI stream on the IP side (S2MM) and all the GPIO AXI that I could find support AXI-lite only. In addition, seems like theres more than one flavor of DMA controllers so Im not sure what the difference is between them all. Is there a specific DMA flavor that supports AXI lite on the IP side as well?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to drozwood90

    Thanks zedman2000, that sounds like the most reasonable solution I've encountered so far. I was also looking into AXI virtual FIFO but it looks like more than I need. Nevertheless, with the DMA solution that you mentioned it seems like the DMA controller hooks up to AXI stream on the IP side (S2MM) and all the GPIO AXI that I could find support AXI-lite only. In addition, seems like theres more than one flavor of DMA controllers so Im not sure what the difference is between them all. Is there a specific DMA flavor that supports AXI lite on the IP side as well?