Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Building image from PetaLinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 901 views
  • Users 0 members are here
Related

Building image from PetaLinux

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I have followed the instruction from this http://www.xilinx.com/support/documentation/sw_manuals/petalinux2013_10/ug980-petalinux-board-bringup.pdf to build image for zedboard. Then I copied the zImage from my build to the SD card that came with the board. I have not touched any other file than zImage. When I boot I get the following error
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>
U-Boot 2011.03-dirty (Jul 11 2012 - 16:07:00)

DRAM:  512 MiB
MMC:   SDHCI: 0
Using default environment

In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 27
OEM: 5048
Name: SD04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 1.10
High Capacity: Yes
Capacity: 3980394496
Bus Width: 1-bit
reading zImage

5872888 bytes read
reading devicetree_ramdisk.dtb

5817 bytes read
reading ramdisk8M.image.gz

3694108 bytes read
## Starting application at 0x00008000 ...

Error: unrecognized/unsupported machine ID (r1 = 0x1fb71dd0).

Available machine support:

ID (hex)        NAME
ffffffff        ARM-Versatile Express
000008e0        ARM-Versatile Express
00000d32        Xilinx Zynq Platform

Please check your kernel config and/or bootloader.
<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<

1. What changes I need to make specific for ZedBoard. I am assuming the instruction were for Xilinx 7000 board.

2. IF there is a problem where can I found the source code to fix it. I don't think petalinux has the full linux source. (I have also built from the Xilinx source tree and it also doesn't work.

Thanks
-

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    Avnet is running a Zynq Petalinux Speedway training now. Check with your local Avnet FAE. The training will be available online here soon.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have finished the PetaLinux board bring up successfully.
    See my "Zynq Design From Scratch" blog for more information:
    http://svenand.blogdrive.com/archive/202.html

    Sven