Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard FMC-IMAGEON strange error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 302 views
  • Users 0 members are here
Related

Zedboard FMC-IMAGEON strange error

e14 Contributor
e14 Contributor over 12 years ago

Hello, I am working with the  FMC-IMAGEON - Building a Video Design from Scratch Tutorial - 14.4 and when I try to test step 3 stop the execution and shows me the following message:

FMC-IMAGEON Initialization ...
HDMI Input Initialization ...
Video Clock Synthesizer Configuration ...
Enabling spread-spectrum clocking (SSC)
type=down-spread, amount=-0.75%
HDMI Output Initialization ...
Video DMA (Output Side) Initialization ...

But if I connect Chipscope ILA to the outputs of VDMA IP everything works perfectly.

I'm using the Zedboard (class D) + the VITA 2000.

Any recommendation to solve this problem will be welcome.

[UPDATE] Just using the instantiation of the Chipscope components (ICON and ILA) is enough to make it work, without these components does not work.

  • Sign in to reply
  • Cancel
  • albertabeef
    0 albertabeef over 12 years ago

    Juan,

    Your system.mhs looks OK.

    Please check that you have the VTC (Video Timing Controller) cores correctly configured:
    - VTC_0 : on the video input side, should have the detection of VSYNC/HSYNC disabled
    - VTC_1 : on the video output side, should be generating all the sync/blank signals
    - AXI4-Stream to Video Ouput : on the video output side, should be configured in master mode

    Here is the solution archive (for ZC702 carrier) for reference:
    t
    FMC_IMAGEON_Building_Video_Design_Tutorial_14_4_20130110_solution.zip
    https://avnet.egnyte.com/h-s/20140129/33f87949d7f6406e

    Regards,

    Mario.