Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Enabling POST in Uboot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 375 subscribers
  • Views 1155 views
  • Users 0 members are here
Related

Enabling POST in Uboot

e14 Contributor
e14 Contributor over 11 years ago

I need to enable the uboot POST for testing memory on the Zed board (Xilinx Zynqu00AE-7000 All-Programmable SoC - ARM dual-core Cortexu2122-A9 + 28 nm programmable logic with Analog Devices AD-FMCOMMS3-EBZ FMC module featuring the AD9361).

Can this be achieved only by modification of the uboot source code ? Or, is there any sequence of keystrokes at the time of booting, for enabling the same?

I added the define directive #define CONFIG_POST  CONFIG_SYS_POST_MEMORY in the zynq_zed.h
file. in directory include/configs of u-boot source(2014.07). But when I built it the following errors are displayed:

1)t_POST_WORD_ADDR currently not implemented for this platform! (file include/post.h).

2)tpost_word_load() undeclared (file include/post.h).

3)tPost_word_store() undeclared (file include/post.h).


What other modifications are required to enable POST ?

- Suresh

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Suresh,

    According to this article, there may be some other #defines that need to be in place for POST to become enabled.

    http://blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:post

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Suresh,

    According to this article, there may be some other #defines that need to be in place for POST to become enabled.

    http://blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:post

    Regards,

    -Kevin