Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SPI Port Access
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 374 subscribers
  • Views 545 views
  • Users 0 members are here
  • mini-module
  • minimodule
  • zynq
  • mini-module_plus
Related

SPI Port Access

e14 Contributor
e14 Contributor over 10 years ago

Newbie alert!

We are currently using the MicroZed board and are looking at the MMP for a new project.

Looking at the Schematic, there are no SPI ports broken out to the connectors as they are on the MicroZed. I understand that the SPI lines can be routed through the EMIO, but looking at the technical reference manual for the Zynq, bank 500 and 501 are already dedicated as QSPI, Ethernet, USB, etc.

Would I need to disable (for example) the QSPI Flash memory to use an SPI port routed through the EMIO, or do they coexist?

Thanks

Craig (newbie)

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Craig,

     

    No, you would not need to disable any of the devices currently using the MIO banks to route the SPI signals to the PL via EMIO. If you take a look at Figure 2.3 in the Zynq Technical Reference you can see that the EMIO connections to the PS SPI controllers are picked off 'before' they go to the MIO Mux.

     

    You would also have the option to implement an SPI interface in the PL using the AXI_Quad_SPI IP. I have found the AXI SPI controller to have fewer limitations than the PS SPI controllers.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi Craig,

    I am going to second Gary's recommendation of using the AXI_QUAD_SPI IP, it is definitely the way to go.  There is a lot more flexibility that the PL SPI controller offers.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thanks Guys.

    That puts my mind at rest. Appreciate it.