Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Boot Baremetal
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 374 subscribers
  • Views 986 views
  • Users 0 members are here
Related

Boot Baremetal

zanabonir
zanabonir over 9 years ago

Dear Forum

I did a  very simple application; led LD9 flah every second usingsome of the Timer available.

The Debug of applcation is working..

Now I would like that zedboard run my app with no jtag connectiontry to boot from QSPI So, following many tutorial, i did:

-Compile my app (Helloword) in release mode

-Create the  FSBL ,using the already created BSP with some library add (the xilffs and xilrsa)

-compile the FSBL in releae.

-So, at this point i have helloword.elf and FSBL.elf in release.

-Now the boot image:

     select Helloword and Xilinxtool-->create boot image

-At end of this ,sdk creates boot.bin and helloword.bif

-Again ->create boot image, and generate helloword.mcs

-Program the flash ,with all chk possible..erease..programm..veryfy ...ALL OK message

-Last,change MIO5 on zedboard for 3.3V ..the only one now in this position

-Restart the zedboard.....NOTHIGN HAPPEND.

-Connecting a serial port and some terminal, have no messages.

The messages via serial port are many ok, apart the lest:

 

 

*****No Execution Address JTAG Handoff*****

 

 

Thanks for help and for was so patient to read this long mail

Roberto

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Robiberto,

    You are following the correct steps to create your .mcs file and programming it in the flash. I have a few questions for you that should help in getting to the bottom of your issue. Have you completed lab 7 of our Zynq Software Speedway where we create a .mcs file and program it into the flash? If you have not, please run through that speedway just to double check that eveyrthing is setup and working properly with your board using the know working example that we provide.

    http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-201441-20152-and-20162

    Also if you are looking at the Software Speedway Lab 7 for Vivado 2016.2, refer to page 4 step 5. That step goes over what should be pre-populated when you create your .mcs file. Did you have all 3 files? If not you may have not selected your application (step 3) prior to creating your boot image or you may need to clean your project.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zanabonir
    0 zanabonir over 9 years ago in reply to jafoste4

    Thanks for reply.....

    yes..the example you show me is working...it can boot...

    My design..(again dont boot.)..is much more simple... it have only the zynq,

    with no external ip (no reset ip for example), and maybe some of them is

    crucial for boot.

    So now i will try to cut the original and see what happend.

    Thanks for reply

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zanabonir
    0 zanabonir over 9 years ago in reply to jafoste4

    Thanks for reply.....

    yes..the example you show me is working...it can boot...

    My design..(again dont boot.)..is much more simple... it have only the zynq,

    with no external ip (no reset ip for example), and maybe some of them is

    crucial for boot.

    So now i will try to cut the original and see what happend.

    Thanks for reply