Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Boot Baremetal
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 374 subscribers
  • Views 986 views
  • Users 0 members are here
Related

Boot Baremetal

zanabonir
zanabonir over 9 years ago

Dear Forum

I did a  very simple application; led LD9 flah every second usingsome of the Timer available.

The Debug of applcation is working..

Now I would like that zedboard run my app with no jtag connectiontry to boot from QSPI So, following many tutorial, i did:

-Compile my app (Helloword) in release mode

-Create the  FSBL ,using the already created BSP with some library add (the xilffs and xilrsa)

-compile the FSBL in releae.

-So, at this point i have helloword.elf and FSBL.elf in release.

-Now the boot image:

     select Helloword and Xilinxtool-->create boot image

-At end of this ,sdk creates boot.bin and helloword.bif

-Again ->create boot image, and generate helloword.mcs

-Program the flash ,with all chk possible..erease..programm..veryfy ...ALL OK message

-Last,change MIO5 on zedboard for 3.3V ..the only one now in this position

-Restart the zedboard.....NOTHIGN HAPPEND.

-Connecting a serial port and some terminal, have no messages.

The messages via serial port are many ok, apart the lest:

 

 

*****No Execution Address JTAG Handoff*****

 

 

Thanks for help and for was so patient to read this long mail

Roberto

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Robiberto,

    I have a suggestion that you could try. Leave your application in Debug instead of Release. In the past I have encountered an issue where my design would work in JTAG when I had my application set to Release, but not  work for QSPI or SD card boot. However, this is just a shot in the dark, it is suggested by most tutorials to modify your applications build confiugrations to Release. Let me know if that helped at all.

    Also, you do not need those IP's that you stated above to do QSPI or SD boot. We have an Reference Design where the only IP we use is a Zynq IP that we load into the QSPI and SD card that works flawlessly for both the MicroZed and PicoZed. It is called "Tutorial 04 FSBL and Boot from QSPI and SD Card" located at:

    http://picozed.org/support/design/13076/106 

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zanabonir
    0 zanabonir over 9 years ago in reply to jafoste4

    Hello

    I try in this days to run Petalinux on zedboard...Today work ...with the boot from

    SD card. But again, the baremetal boot dont work.

    Do some have a BOOT.bin file of some simple baremetal, flashing some led

    or similar..already tested.I want only to copy-paste on my SD

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zanabonir
    0 zanabonir over 9 years ago in reply to jafoste4

    Hello

    I try in this days to run Petalinux on zedboard...Today work ...with the boot from

    SD card. But again, the baremetal boot dont work.

    Do some have a BOOT.bin file of some simple baremetal, flashing some led

    or similar..already tested.I want only to copy-paste on my SD

     

    Thanks