Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Passing MAC address to kernel via Device Tree Blob
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 374 subscribers
  • Views 10023 views
  • Users 0 members are here
Related

Passing MAC address to kernel via Device Tree Blob

e14 Contributor
e14 Contributor over 13 years ago

Good morning everyone,

in our lab, we have several ZedBoards of which some obtain an IP address from a DHCP server based on their MAC address and some of them use a fixed IP address (no DHCP).

Based on my experience with other embedded Linux boards, the straight forward solution to achieve this would be to generate an individual device tree source (DTS) file for each board containing
- the specific MAC address and
- the specific boot arguments for the kernel to either turn on DHCP or to assign a specific fixed IP address.

According to the Embedded Linux Hands-on Tutorial and the Embedded Linux Development Guide, it is recommended to set the MAC address of the ethernet port of the ZedBoard via U-Boot (zynq_zed.h). However, it is also mentioned that the MAC address can be set via DTS file. To do so, the MAC address assignment in the U-Boot configuration needs to be deleted.

Now to my problem:
If I now boot the ZedBoard with such a configuration, the MAC address of the system differs from the address specified in the DTS file. More precisely, the first 4 Bytes are equal to the specified address but the last 2 Bytes are always zero.
Example:
AA:BB:CC:DD:11:FF -> AA:BB:CC:DD:00:00

If the MAC address is set via U-Boot, everything is fine. Except that I then need to generate both a specific BOOT.BIN (containing the U-Boot) and a DTS file for each board.

I think that there is an error in how the MAC address is passed from the DTS to the driver (xemacps). Does anyone of you have an idea how to fix that?

Best regards,

Pirmin

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 10 years ago

    Hi Paul,

    I cannot say that I have ever tried this under Ubuntu and I am not sure what would cause eth0 to not come up after changing ethaddr under U-Boot.

    Have you checked your device tree to see if there is a 00:0a:35:00:01:22 entry for your Ethernet interface in there?

    Thanks for the note about the stale Ethernet address being used until the system is rebooted, I did not catch that during my experiment.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 10 years ago

    Hi Paul,

    I cannot say that I have ever tried this under Ubuntu and I am not sure what would cause eth0 to not come up after changing ethaddr under U-Boot.

    Have you checked your device tree to see if there is a 00:0a:35:00:01:22 entry for your Ethernet interface in there?

    Thanks for the note about the stale Ethernet address being used until the system is rebooted, I did not catch that during my experiment.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • paulclaessen
    0 paulclaessen over 10 years ago in reply to zedhed

    Kevin,

    Thanks for your response.

    No, I haven't checked my device tree (I'm getting my BOOT.bin blob from someone else, and I would have to check with this person), but as you yourself proved at the beginning of this thread, the uBoot ethaddress environment variable overwrites what's in the device tree.

    (Note, btw, that uBoot now DOES let you change the ethaddress variable as described in my previous message: a lot of articles I found claim that once it's set, uBoot won't allow you to change it anymore .. that appears to no longer be the case .. thankfully)

    (Note2: this also raises the question: if the env variable overwrites the device tree's MAC address, where (and by whom) is this uBooot env variable set initially?)

    Btw, I also tried simply setting the mac address with ifconfig: to my surprise, this actually worked:
    ifconfig eth0 down
    ifconfgi eth0 hw ether <mac address>
    ifconfig eth0 up

    UNfortunately, the interface doesn't work anymore after that, I get the error (on a simple ping):
    connect: Network is unreachable

    I would expect maybe some problems at the receiving end (the gateway for instance), because it still has the old MAC address for our IP address in its arp table, but that should be resolved in a few minutes), but the above error clearly indicates something got messed up at the sending side (us!).

    ANYWAY ... I have read other posts about this, following some of the links you have provided, but the main basic question remains:

    In a production environment, using Zynq 7000 based systems like the Zed board, what is the most efficient way to get every device its own unique MAC address?
    Setting a MAC address as a uBoot env variable is an acceptable solution.
    Clearly, generating a unique device tree and thus building a new BOOT.bin blob for every single device is not. ;-)

    It's actually a real problem now, since we have two Zedboard that are being worked with, and they both have the same MAC address, which causes issues.

    ~ Paul Claessen