Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General USB-JART not recognized
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 373 subscribers
  • Views 852 views
  • Users 0 members are here
Related

USB-JART not recognized

e14 Contributor
e14 Contributor over 12 years ago

I have installed tye Cypress driver and configured it in Tera Term, but still, I couldn't see the LED light on and the sdk is not able to detect jtag...I'm wondering if anyone has any idea how to solve this?

Under Device Manager, instead of Cypress USB to UART Adapter, I have USB to UART adapter only, but when I click on it I still see the driver being Cypress, so I'm not sure if it could be an issue or not...

Other than that I couldn't think of any...I plugged it into PROG port and it worked fine..

I followed every step in this guide

www.zedboard.org/sites/default/files/documentations/CY7C64225_Setup_Guide_1_3.pdf

and it still wouldn't work, I also tried to re-install the device and driver, no luck either, my system is Windows 7

I am pretty clueless now...any help would be appreciated!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Make sure your TeraTerm session is set to serial, 115200, and that the COM port matches the one assigned to the USB-UART driver shown in Windows Device Manager.

     

    Have you tried booting the ZedBoard using the image provided on the SD Card.?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Some more details:

    So I could see the LEDS(green, blud, amber)

    the green and amber LEDS flash for a bit and then disappeared

    on terminal I'm stucked at

    [0.00000] console [tty0] enabled, bootconsole disabled

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Some more details:

    So I could see the LEDS(green, blud, amber)

    the green and amber LEDS flash for a bit and then disappeared

    on terminal I'm stucked at

    [0.00000] console [tty0] enabled, bootconsole disabled