Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Speedway Lab2, Experiment 4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 320 views
  • Users 0 members are here
Related

Speedway Lab2, Experiment 4

e14 Contributor
e14 Contributor over 13 years ago

I got to the point in the lab where I had selected the standalone OS configuration in the SDK.  All dialog selections were per the instructions.

The build began as soon as I OK'd the dialog.

The build did NOT succeed.  The console output from the SDK is shown here:

make -k all
libgen -hw ../system_hw_platform/system.xml
t      
t       -pe ps7_cortexa9_0
t       -log libgen.log
t       system.mss
libgen
Xilinx EDK 14.4 Build EDK_P.49d
Copyright (c) 1995-2012 Xilinx, Inc.  All rights reserved.

Command Line: libgen -hw ../system_hw_platform/system.xml -pe ps7_cortexa9_0
-log libgen.log system.mss


Staging source files.
Running DRCs.
Running generate.
Running post_generate.
Running include - 'make -s include "COMPILER=arm-xilinx-eabi-gcc"
"ARCHIVER=arm-xilinx-eabi-ar" "COMPILER_FLAGS= -O2 -c"
"EXTRA_COMPILER_FLAGS=-g"'.

Running libs - 'make -s libs "COMPILER=arm-xilinx-eabi-gcc"
"ARCHIVER=arm-xilinx-eabi-ar" "COMPILER_FLAGS= -O2 -c"
"EXTRA_COMPILER_FLAGS=-g"'.
"Compiling xadc"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling standalone"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -march=armv7-a -mfloat-abi=soft -mfpu=neon -I./. -I../../../include _exit.c _open.c _sbrk.c abort.c close.c errno.c fcntl.c fstat.c getpid.c inbyte.c isatty.c kill.c lseek.c open.c outbyte.c print.c putnum.c read.c sbrk.c sleep.c smc.c uart.c unlink.c usleep.c vectors.c write.c xil_assert.c xil_cache.c xil_exception.c xil_io.c xil_mmu.c xil_printf.c xil_testcache.c xil_testio.c xil_testmem.c xl2cc_counter.c xpm_counter.c xtime_l.c asm_vectors.S boot.S cpu_init.S translation_table.s xil-crt0.S, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [standalone_libs] Error 2
make[1]: Target `libs' not remade because of errors.
"Compiling devcfg"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling dmaps"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling scugic"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling scutimer"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling scuwdt"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling uartps"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling cpu_cortexa9"
ERROR:EDK:369 -  make failed for target "libs"
ERROR:EDK:3418 - Error(s) while running make.
make: *** [ps7_cortexa9_0/lib/libxil.a] Error 2
make: Target `all' not remade because of errors.


Is this a path problem of some kind?

This is the location of standalone_bsp_0:
C:SppedwayFall_12Zync_IntroLED_ControllerLED_Controller.sdkSDKSDK_Exportstandalone_bsp_0

This is the location of 'system_hw_platform':
C:SppedwayFall_12Zync_IntroLED_ControllerLED_Controller.sdkSDKSDK_Exportsystem_hw_platform

The 'system_hw_platform' folder IS populated with the exported 'ps7_init.c' and 'ps7_init.h' files from the ealier export.

Thanks,
Bill

warkatzed

  • Sign in to reply
  • Cancel
Parents
  • jamestkennedy
    0 jamestkennedy over 13 years ago

    MT41J128M16HA-15E.
    From
    Zynqu2122Evaluation and Development
    Hardware Useru2019s Guide:

    2.2.1 DDR3
    The ZedBoard includes two Micron MT41J128M16HA-15E:D DDR3 memory components creating a 32-bit interface. As of August 2012, this device has been marked by Micron for end-of-life. There are several options that Micron offers for a replacement. ZedBoard will likely migrate to the MT41K128M16JT-125 device, although this is pending validation. The DDR3 is connected to the hard memory controller in the Processor Subsystem (PS) as outlined in the Zynq datasheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jamestkennedy
    0 jamestkennedy over 13 years ago

    MT41J128M16HA-15E.
    From
    Zynqu2122Evaluation and Development
    Hardware Useru2019s Guide:

    2.2.1 DDR3
    The ZedBoard includes two Micron MT41J128M16HA-15E:D DDR3 memory components creating a 32-bit interface. As of August 2012, this device has been marked by Micron for end-of-life. There are several options that Micron offers for a replacement. ZedBoard will likely migrate to the MT41K128M16JT-125 device, although this is pending validation. The DDR3 is connected to the hard memory controller in the Processor Subsystem (PS) as outlined in the Zynq datasheet.