Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General U-boot machine ID
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 373 subscribers
  • Views 1775 views
  • Users 0 members are here
Related

U-boot machine ID

e14 Contributor
e14 Contributor over 13 years ago

Currently I am testing the zedboard's zynq chip for its potential use in future products.
One of its requirements is to run Windriver Linux, this is giving quite the problems.


After creating a new linux kernel, devicetree and rootfs, I use the xilinx U-Boot to launch this new kernel.


I can launch the original linuz that came with the board using this U-Boot. With my own kernel it gets stuck after 'booting the kernel'.


Now this isnt the most uncommon error and using low-level debugging I managed to extract the following onformation:
<6>Booting Linux on physical CPU 0
<6>Initializing cgroup subsys cpuset
<6>Initializing cgroup subsys cpu
<5>Linux version 3.4.34-rt40-WR5.0.1.0_preempt-rt (gcc version 4.6.3 (Wind River Linux Sourcery CodeBench 4.6a-99) ) #1 SMP PREEMPT RT Tue May 7 10:05:01 CEST 2013
<4>CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
<4>CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
<4>
<4>Error: unrecognized/unsupported machine ID (r1 = 0x1fb56824).
<4>
<4>Available machine support:
<4>
<4>ID (hex)tNAME
<4>fffffffftXilinx Zynq Platform
<4>
<4>Please check your kernel config and/or bootloader.



after a long struggle to find out the problem, it appears that U-Boot is not giving a correct machine ID (the r1) to the kernel.


So the zedlinux does not require this check? is that some sort of config that I can set in my own kernel as well?
I checked the machine ID that the U-Boot creates/finds using dbinfo.
This machine id is identical to the r1 of the error message.


In the xilinx U-boot repository the correct machine ID can be found in mach-types.h but this does not appear to be used by the zynq config. Is this perhaps the problem? Or can I create a new U-Boot that does contain the correct ID?

  • Sign in to reply
  • Cancel
Parents
  • linux.matthew
    0 linux.matthew over 12 years ago

    Has there been a solution for this?  I can boot off an SD card I create with the u-boot kernel image I bitbake from the meta-xilinx layer.  But if I try to bootp/bootm the kernel, it dies with the error described above

    Error: unrecognized/unsupported machine ID (r1 = 0x00000000).

    Available machine support:

    ID (hex)        NAME
    ffffffff        ARM-Versatile Express
    000008e0        ARM-Versatile Express
    00000d32        Xilinx Zynq Platform

    How can I get around this?

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • linux.matthew
    0 linux.matthew over 12 years ago

    Has there been a solution for this?  I can boot off an SD card I create with the u-boot kernel image I bitbake from the meta-xilinx layer.  But if I try to bootp/bootm the kernel, it dies with the error described above

    Error: unrecognized/unsupported machine ID (r1 = 0x00000000).

    Available machine support:

    ID (hex)        NAME
    ffffffff        ARM-Versatile Express
    000008e0        ARM-Versatile Express
    00000d32        Xilinx Zynq Platform

    How can I get around this?

    Matt