Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Xillinux xillydemo edit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 373 subscribers
  • Views 858 views
  • Users 0 members are here
Related

Xillinux xillydemo edit

deaxman
deaxman over 13 years ago

How should I edit Xillydemo if I want to store values to user_r_mem_8_data to be read back in the terminal window? (Under /dev)  I know that xillydemo uses demoarray to store to this user_r_mem_8_data register.  Is the accepted practice to save what I want to demoarray?  should I do it on the bus clock or another clock?  Thanks a ton!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    I'm afraid I can't figure out what you want to accomplish, so I'll try some general comments.

    It's perfectly OK to read from /dev/xillybus_mem_8 as a sequential file. Using hexdump -C -n 32 /dev/xillybus_mem_8 will print out the first (actually, all) 32 bytes in the array. This relies on that a newly opened file always starts on address 0.

    So this is a simple way to print out the data to the terminal window.

    As for clocking: demoarray[] is an inferred synchronous RAM. You may replace it with a dual-clock RAM (inferred or explicitly instantiated) if you want to access its content with another clock. The side interfacing with the Xillybus IP core must be clocked with bus_clk however.

    I hope this helps.
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deaxman
    0 deaxman over 13 years ago in reply to e14 Contributor

    Thanks!  Your reply was very helpful for the terminal side of the connection!  I should have specified in my question though that right now I'm trying to create the bit file to write to the FPGA.  This is being done as specified in the directions here: xillybus_getting_started_zynq       and it was recommended that I modify the xillydemo.v file and write to the user_r_mem_8_data register in verilog (or vhdl).  So I'm just not sure how to send the values into the register to be brought to the /dev folder.  Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • deaxman
    0 deaxman over 13 years ago in reply to e14 Contributor

    Thanks!  Your reply was very helpful for the terminal side of the connection!  I should have specified in my question though that right now I'm trying to create the bit file to write to the FPGA.  This is being done as specified in the directions here: xillybus_getting_started_zynq       and it was recommended that I modify the xillydemo.v file and write to the user_r_mem_8_data register in verilog (or vhdl).  So I'm just not sure how to send the values into the register to be brought to the /dev folder.  Thanks!