Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Smart vision developpement kit boot/ problem running SW app
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 443 views
  • Users 0 members are here
Related

Smart vision developpement kit boot/ problem running SW app

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I just got a Smart Vision Developpement Kit featuring Picozed board with 7015 Zynq and I am struggling with a problem when trying to test my first design.
For now I just want to run a few GPIOs, open and send info via a COM link (UART).

By default the board is booting from an application stored on QSPI which  transmits via GigE image from the camera (Sensor 2 image reference design).

When I try to program the FPGA HW from the vivado HW manager I have no change on my output (EMIO state), even though the programation is said succesfull into Vivado. There is no change.

So what I did is try to use only the SDK and there same thing I tried program FPGA and run application and it did not work.

I tried to run only the SW application and my application is not launched most of the time (I turn on a led on the board). Sometime I get error message like impossible to run ps7_init, sometime process keep running, sometime no error just no output.
What is weird is that from time to time I am successfull launching the SW application (led turn on and off), I was not able to understand why it worked at those time and not before.

Once SW app has been sucessfully launched once, I can program the PL part (this time I get EMIO pins which go low after download) and run SW  again which in addition to light a led on the board also turns on and off 2 EMIOS output pins at same time. At this stage if I don't switch off my board I can change SW or HW programmation and it works good (though COM link is still not working for some other reasons probably). I was able to implement at that time a I2C control of a external device and it was working fine.
Problem appears again when I finaly switch off my board. I spend a few hours trying to program my board again and to understand why it works only from time to time several times already. 

For now what I understand is that:
-The QSPI app once launched on the board (and working) prevent most of the time any launch of the SW).
-In order to be able to program my HW I must have launched my SW app once.


I must precise that I had a Microzed board for a few days before and I never had this kind of trouble with it. COM link as well was working fine.

Thanks for your help.
Ben

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I take the oppportunity to post a last time on this topic as Xilinx FAE help me to solve out my problem. In fact their were two cause to my problems:
            -default DDR preset which were incorrect were generating a bug into my design (even though DDR was not used in my code). We deactivated the DDR and it solved the problem.
            -Linker script was not correct and needed to be regenerated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I take the oppportunity to post a last time on this topic as Xilinx FAE help me to solve out my problem. In fact their were two cause to my problems:
            -default DDR preset which were incorrect were generating a bug into my design (even though DDR was not used in my code). We deactivated the DDR and it solved the problem.
            -Linker script was not correct and needed to be regenerated.