Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Speed of serial links on FMC connector
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 362 views
  • Users 0 members are here
Related

Speed of serial links on FMC connector

erichnast
erichnast over 9 years ago

Do you have any specs on the speed of the serial links on the FMC connectors.  I would like to use the 4DSP FMC104 module

http://www.4dsp.com/FMC104.php

Want to use the  configurationLVDS

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Erich Nast,

    The FMC connector is rated properly for running any of the SOMs that we have to plug into the boards they are populated on. 

    For example, the connector on the PicoZed FMCv2 is routed and pinned for running as fast as the Zynq 7030 GTX Transceivers. The FMC connector is not technically "rated" for a specific number, but a tolerance to dB loss over frequence. 

    So a general rule of thumb is, depending on what board you are using of ours, it is rated to run at the speed of the transceivers for the transceiver pins, and then as fast as the pins for the LVDS Pairs for any other pin(950 MBps). Please refer to the PicoZed 7015/7030 Hardware user guide section 2.8.1 http://zedboard.org/support/documentation/4736

    So to answer your question, it depends on which board you are using.

    --Josh