Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SD Init failed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 742 views
  • Users 0 members are here
Related

SD Init failed

e14 Contributor
e14 Contributor over 11 years ago

Hello I am trying to boot from SD and i have done that successfully before on same SD card. what happening is this following message from fsbl code .


Boot mode is SD
SD_INIT_FAIL
FSBL Status = 0xa009

This Boot Mode Doesn't Support Fallback

So please any help what I can should do ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

      Perhaps you are doing this already, but first load a known good BOOT.BIN file for the target you are using on the SD card.  You can download any of the reference designs on this site for your target to obtain one.  Note that the file must be named BOOT.BIN, or the BOOTROM code in the Zynq will not be able to locate it and you will get the error you are seeing.

    If you have done this, then try using a different SD card, formatted FAT32, with your BOOT.BIN file loaded.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    hello thanks for your reply,
    I have started new project and formatted the SD to FAT32 and got the same error. I also tried the previous project which its BOOT file worked and it ran successfully. I also got the error from Sd.c and it is as follows :
    Boot mode is SD
    SD: rc= 00000000
    SD: Unable to open file BOOT.BIN: 3
    SD_INIT_FAIL
    FSBL Status = 0xa009

    do I need to do something more.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    SOLVED
    IT WAS voltage bank problem
    I should put voltage bank 1.8 V while I was putting it 3.3V in the MIO design. So I think SD need 1.8 V not 3.3V to work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    SOLVED
    IT WAS voltage bank problem
    I should put voltage bank 1.8 V while I was putting it 3.3V in the MIO design. So I think SD need 1.8 V not 3.3V to work