Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General hdmi not registered
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 374 subscribers
  • Views 664 views
  • Users 0 members are here
Related

hdmi not registered

e14 Contributor
e14 Contributor over 10 years ago

U-Boot 2014.01 (May 02 2016 - 17:05:24)

I2C:   ready
Memory: ECC disabled
DRAM:  512 MiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  0
zynq-uboot> boot
Device: zynq_sdhci
Manufacturer ID: 27
OEM: 5048
Name: SD04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading uEnv.txt
** Unable to read file uEnv.txt **
Copying Linux from SD to RAM...
reading uImage
3232000 bytes read in 323 ms (9.5 MiB/s)
reading devicetree.dtb
10872 bytes read in 16 ms (663.1 KiB/s)
## Booting kernel from Legacy Image at 03000000 ...
   Image Name:   Linux-3.18.0-ge723d64-dirty
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3231936 Bytes = 3.1 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02a00000
   Booting using the fdt blob at 0x2a00000
   Loading Kernel Image ... OK
   Loading Device Tree to 1fb28000, end 1fb2da77 ... OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0x0
Linux version 3.18.0-ge723d64-dirty (root@linux32) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #10 SMP PREEMPT Mon May 2 16:03:57 IST 2016
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Xilinx Zynq ZED
bootconsole [earlycon0] enabled
cma: Reserved 128 MiB at 0x17800000
Memory policy: Data cache writealloc
PERCPU: Embedded 9 pages/cpu @dfb9a000 s8128 r8192 d20544 u36864
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 381692K/524288K available (4322K kernel code, 246K rwdata, 1668K rodata, 208K init, 144K bss, 142596K reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xffe00000   (2048 kB)
    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc05e1c68   (5992 kB)
      .init : 0xc05e2000 - 0xc0616000   ( 208 kB)
      .data : 0xc0616000 - 0xc06538c0   ( 247 kB)
       .bss : 0xc06538c0 - 0xc06779ec   ( 145 kB)
Preemptible hierarchical RCU implementation.
        Dump stacks of tasks blocking RCU-preempt GP.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 1 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 8 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76360001
slcr mapped to e0804000
zynq_clock_init: clkc starts at e0804100
Zynq clock init
sched_clock: 16 bits at 54kHz, resolution 18432ns, wraps every 1207951633ns
timer #0 at e0806000, irq=43
Console: colour dummy device 80x30
Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x414500 - 0x414558
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated.
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
zynq_get_revision: no devcfg node found
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
zynq-ocm f800c000.ps7-ocm: ZYNQ OCM pool: 256 KiB @ 0xe0880000
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
media: Linux media interface: v0.10
Linux video capture interface: v2.00
EDAC MC: Ver: 3.0.0
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource ttc_clocksource
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
futex hash table entries: 512 (order: 3, 32768 bytes)
msgmni has been set to 1001
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
dma-pl330 f8003000.ps7-dma: Loaded driver for PL330 DMAC-241330
dma-pl330 f8003000.ps7-dma:     DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
xuartps e0001000.uart: ttyPS0 at MMIO 0xe0001000 (irq = 82, base_baud = 3125000) is a xuartps
u00E0console [ttyPS0] enabled
console [ttyPS0] enabled
bootconsole [earlycon0] disabled
bootconsole [earlycon0] disabled
[drm] Initialized drm 1.1.0 20060810
drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.c:axi_hdmi_platform_probe[176]
platform 70e00000.axi_hdmi: Driver axi-hdmi requests probe deferral
brd: module loaded
loop: module loaded
m25p80 spi32766.0: found s25fl256s1, expected n25q128a11
m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
5 ofpart partitions found on MTD device spi32766.0
Creating 5 MTD partitions on "spi32766.0":
0x000000000000-0x000000500000 : "boot"
0x000000500000-0x000000520000 : "bootenv"
0x000000520000-0x000000540000 : "config"
0x000000540000-0x000000fc0000 : "image"
0x000000fc0000-0x000002000000 : "spare"
libphy: XEMACPS mii bus: probed
xemacps e000b000.eth: pdev->id -1, baseaddr 0xe000b000, irq 54
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ULPI transceiver vendor/product ID 0x0451/0x1507
Found TI TUSB1210 ULPI transceiver.
ULPI integrity check: passed.
zynq-ehci zynq-ehci.0: Xilinx Zynq USB EHCI Host Controller
zynq-ehci zynq-ehci.0: new USB bus registered, assigned bus number 1
zynq-ehci zynq-ehci.0: irq 53, io mem 0x00000000
zynq-ehci zynq-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
zynq-edac f8006000.ps7-ddrc: ecc not enabled
Xilinx Zynq CpuIdle Driver started
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-arasan e0100000.sdhci: No vmmc regulator found
sdhci-arasan e0100000.sdhci: No vqmmc regulator found
mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
ledtrig-cpu: registered to indicate activity on CPUs
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
adv7511-hdmi-snd fpga-axi@0:adv7511_hdmi_snd: ASoC: CODEC DAI adv7511 not registered
platform fpga-axi@0:adv7511_hdmi_snd: Driver adv7511-hdmi-snd requests probe deferral
zed-adau1761-snd fpga-axi@0:zed_sound: ASoC: CODEC DAI adau-hifi not registered
platform fpga-axi@0:zed_sound: Driver zed-adau1761-snd requests probe deferral
TCP: cubic registered
NET: Registered protocol family 17
Registering SWP/SWPB emulation handler
drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.c:axi_hdmi_platform_probe[197]
mmc0: new high speed SDHC card at address 0007
mmcblk0: mmc0:0007 SD04G 3.70 GiB
mmcblk0: p1 p2
platform 70e00000.axi_hdmi: Driver axi-hdmi requests probe deferral
adv7511-hdmi-snd fpga-axi@0:adv7511_hdmi_snd: ASoC: CODEC DAI adv7511 not registered
platform fpga-axi@0:adv7511_hdmi_snd: Driver adv7511-hdmi-snd requests probe deferral
zed-adau1761-snd fpga-axi@0:zed_sound: ASoC: CODEC DAI adau-hifi not registered
platform fpga-axi@0:zed_sound: Driver zed-adau1761-snd requests probe deferral
drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.c:axi_hdmi_platform_probe[197]
platform 70e00000.axi_hdmi: Driver axi-hdmi requests probe deferral
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
ALSA device list:
  No soundcards found.
usb 1-1: new low-speed USB device number 2 using zynq-ehci
input:  USB OPTICAL MOUSE as /devices/soc0/amba@0/e0002000.usb/zynq-ehci.0/usb1/1-1/1-1:1.0/0003:15D9:0A4C.0001/input/input0
hid-generic 0003:15D9:0A4C.0001: input,hidraw0: USB HID v1.11 Mouse [ USB OPTICAL MOUSE] on usb-zynq-ehci.0-1/input0
adv7511-hdmi-snd fpga-axi@0:adv7511_hdmi_snd: ASoC: CODEC DAI adv7511 not registered
platform fpga-axi@0:adv7511_hdmi_snd: Driver adv7511-hdmi-snd requests probe deferral
zed-adau1761-snd fpga-axi@0:zed_sound: ASoC: CODEC DAI adau-hifi not registered
platform fpga-axi@0:zed_sound: Driver zed-adau1761-snd requests probe deferral
drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.c:axi_hdmi_platform_probe[197]
platform 70e00000.axi_hdmi: Driver axi-hdmi requests probe deferral
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 208K (c05e2000 - c0616000)
u00FFu00CDBu00BAu00A2JZu00A5u00B1u00B1u00E5UMu00A5u00B9u00B1init: ureadahead main process (727) terminated with status 5
Last login: Thu Jan  1 00:00:09 UTC 1970 on tty1
cat: /var/lib/update-notifier/fsck-at-reboot: No such file or directory
run-parts: /etc/update-motd.d/98-fsck-at-reboot exited with return code 1
Welcome to Linaro 12.09 (GNU/Linux 3.18.0-ge723d64-dirty armv7l)

* Documentation:  https://wiki.linaro.org/

0 packages can be updated.
0 updates are security updates.

root@linaro-ubuntu-desktop:~#

please help me sir

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 10 years ago

    Hi babuji,

    Which target board are you running Ubuntu on?

    Is this being done on a Xilinx ZC702 board?

    http://www.xilinx.com/products/boards-and-kits/ek-z7-zc702-g.html

    Or is this being done on an Avnet ZedBoard?

    http://zedboard.org/

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 10 years ago

    Hi babuji,

    Which target board are you running Ubuntu on?

    Is this being done on a Xilinx ZC702 board?

    http://www.xilinx.com/products/boards-and-kits/ek-z7-zc702-g.html

    Or is this being done on an Avnet ZedBoard?

    http://zedboard.org/

    Regards,

    -Kevin