Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General distinguish MicroZed-7010 from -7020 from Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 373 subscribers
  • Views 334 views
  • Users 0 members are here
Related

distinguish MicroZed-7010 from -7020 from Linux

e14 Contributor
e14 Contributor over 9 years ago

I have .bin files to load PL into the MicroZed-7010, and the MicroZed-7020.  I would like to determine from Pulsar Linux which type of board I'm running on, so I can load the correct .bin file.  uname doesn't seem to provide any help.

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Mooney,

    I was able to find a Zynq register 'PSS_IDCODE' that has the information to determine where it is a Zynq 7010 or 7020.

    http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf (page 1638)

    I then verified that I could in deed read the register and determine the zynq device type from XMD in the SDK.

    The issue you may find with this is finding a way to read this register from Pulsar Linux. Unless this is somthing that is already exposed via /proc/ I am unaware of a way to get this information into Pulsar Linux except for writing a full up driver to read this register value.

    You could possible read this register value from U-Boot and then write it into QSPI Flash as a possible work around.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Mooney,

    I was able to find a Zynq register 'PSS_IDCODE' that has the information to determine where it is a Zynq 7010 or 7020.

    http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf (page 1638)

    I then verified that I could in deed read the register and determine the zynq device type from XMD in the SDK.

    The issue you may find with this is finding a way to read this register from Pulsar Linux. Unless this is somthing that is already exposed via /proc/ I am unaware of a way to get this information into Pulsar Linux except for writing a full up driver to read this register value.

    You could possible read this register value from U-Boot and then write it into QSPI Flash as a possible work around.

    --Josh