Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General AES-FMC-HDMI-CAM-G Tutorials
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 1245 views
  • Users 0 members are here
Related

AES-FMC-HDMI-CAM-G Tutorials

slm130430
slm130430 over 9 years ago

Hello - My project is to do video processing with the Zedboard Zynq-7000 SoC. We have implemented our convolution architecture using Vivado 2016.2 and are now focusing on the video I/O portion. To facilitate HDMI input and output, we ordered the AES-FMC-HDMI-CAM-G module. Here is the link for the module:

https://products.avnet.com/shop/en/ProductDisplay?storeId=715839035&catalogId=10001&langId=-1&productId=3074457345628965509

1. In attempting the tutorials on the product page, we are encountering a number of issues. First question: Can we use ANY HDMI (unencrypted) source with this module, or does it only support certain cameras? I note the product page identifies two "related parts": (a) the AES-CAM-ON-P1300C-G ON Semiconductor PYTHON-1300-Color Camera, and (b) the AES-CAM-TOSH-1080P-G Toshiba Industrial 1080P60 Camera Module. We are not using either of these cameras, nor do we want to. 

2. Are there any in-depth tutorials for the FMC-HDMI-CAM-G module in addition to the ones linked to on the product page?

Many thanks, Stuart

  • Sign in to reply
  • Cancel
  • albertabeef
    0 albertabeef over 9 years ago

    Stuart,

    Any non-encrypted DVI or HDMI video source should work with the FMC-HDMI-CAM's HDMI input.

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • axi130430
    0 axi130430 over 9 years ago

    Hello, 

    I understand that the AES-FMC-HDMI-CAM-G is the successor to the FMC-Imageon, however, it seems that the two products are similar. Would it be correct to say that you could follow the Imageon tutorial, and use the IMAGEON IPs,  for the AES-FMC-HDMI-CAM-G? Some links for example are below:
     

    Camera tutorial for FMC-IMAGEON

    https://source.ece.iastate.edu/scm/viewvc.php/*checkout*/MP-2/docs/Camera/FMC-IMAGEON-Tutorial.pdf?root=cpre488

    Getting started for FMC-IMAGEON:

    http://community.avnet.com/avnet/attachments/avnet/FMCHDMIIOVITAImageSensor/420/1/FMC_IMAGEON_GettingStarted_2014_4-Tutorial.pdf

     

    I would appreciate if you could lead me into the right direction.

    -Amann