Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 337 views
  • Users 0 members are here
Related

SDK

sarah_shabani@rocketmail.com
sarah_shabani@rocketmail.com over 9 years ago

Hi, I am trying to create my first project SDK with example Zedboard following:

============================================================================================================
/*
* Copyright (c) 2009 Xilinx, Inc. All rights reserved.
*
* Xilinx, Inc.
* XILINX IS PROVIDING THIS DESIGN, CODE, OR INFORMATION "AS IS" AS A
* COURTESY TO YOU. BY PROVIDING THIS DESIGN, CODE, OR INFORMATION AS
* ONE POSSIBLE IMPLEMENTATION OF THIS FEATURE, APPLICATION OR
* STANDARD, XILINX IS MAKING NO REPRESENTATION THAT THIS IMPLEMENTATION
* IS FREE FROM ANY CLAIMS OF INFRINGEMENT, AND YOU ARE RESPONSIBLE
* FOR OBTAINING ANY RIGHTS YOU MAY REQUIRE FOR YOUR IMPLEMENTATION.
* XILINX EXPRESSLY DISCLAIMS ANY WARRANTY WHATSOEVER WITH RESPECT TO
* THE ADEQUACY OF THE IMPLEMENTATION, INCLUDING BUT NOT LIMITED TO
* ANY WARRANTIES OR REPRESENTATIONS THAT THIS IMPLEMENTATION IS FREE
* FROM CLAIMS OF INFRINGEMENT, IMPLIED WARRANTIES OF MERCHANTABILITY
* AND FITNESS FOR A PARTICULAR PURPOSE.
*
* helloworld.c: simple test application
*/
#include <stdio.h>
#include "platform.h"
#include "xil_types.h"
#include "xgpio.h"
#include "xtmrctr.h"
#include "xparameters.h"
#include "xgpiops.h"
#include "xil_io.h"
#include "xil_exception.h"
#include "xscugic.h"
static XGpioPs psGpioInstancePtr;
extern XGpioPs_Config XGpioPs_ConfigTable[XPAR_XGPIOPS_NUM_INSTANCES];
static int iPinNumber = 7; /*Led LD9 is connected to MIO pin 7*/
XScuGic InterruptController; /* Instance of the Interrupt Controller */
static XScuGic_Config *GicConfig;/* The configuration parameters of the
controller */
static int InterruptFlag;
extern char inbyte(void);

void Timer_InterruptHandler(void *data, u8 TmrCtrNumber)
{
print("\r\n");
print("\r\n");
print("@@@@@@@@@@@@@@@@@@@@@@@@@@@@@\r\n");
print(" Inside Timer ISR \n \r ");
XTmrCtr_Stop(data,TmrCtrNumber);
// PS GPIO Writing
print("LED 'LD9' Turned ON \r\n");
XGpioPs_WritePin(&psGpioInstancePtr,iPinNumber,1);
XTmrCtr_Reset(data,TmrCtrNumber);
print(" Timer ISR Exit\n \n \r");
print("@@@@@@@@@@@@@@@@@@@@@@@@@@@@@\r\n");
print("\r\n");
print("\r\n");
InterruptFlag = 1;
}

int SetUpInterruptSystem(XScuGic *XScuGicInstancePtr)
{
/*
* Connect the interrupt controller interrupt handler to the hardware
* interrupt handling logic in the ARM processor.
*/
Xil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,
(Xil_ExceptionHandler) XScuGic_InterruptHandler,
XScuGicInstancePtr);
/*
* Enable interrupts in the ARM
*/
Xil_ExceptionEnable();
return XST_SUCCESS;
}

int ScuGicInterrupt_Init(u16 DeviceId,XTmrCtr *TimerInstancePtr)
{
int Status;
/*
* Initialize the interrupt controller driver so that it is ready to
* use.
*/
GicConfig = XScuGic_LookupConfig(DeviceId);
if (NULL == GicConfig) {
return XST_FAILURE;
}
Status = XScuGic_CfgInitialize(&InterruptController, GicConfig,
GicConfig->CpuBaseAddress);
if (Status != XST_SUCCESS) {
return XST_FAILURE;
}
/*
* Setup the Interrupt System
*/
Status = SetUpInterruptSystem(&InterruptController);
if (Status != XST_SUCCESS) {
return XST_FAILURE;
}
/*
* Connect a device driver handler that will be called when an
* interrupt for the device occurs, the device driver handler performs
* the specific interrupt processing for the device
*/
Status = XScuGic_Connect(&InterruptController,
XPAR_FABRIC_AXI_TIMER_1_INTERRUPT_INTR,
(Xil_ExceptionHandler)XTmrCtr_InterruptHandler,
(void *)TimerInstancePtr);
if (Status != XST_SUCCESS) {
return XST_FAILURE;
}
/*
* Enable the interrupt for the device and then cause (simulate) an
* interrupt so the handlers will be called
*/
XScuGic_Enable(&InterruptController, XPAR_FABRIC_AXI_TIMER_1_INTERRUPT_INTR);
return XST_SUCCESS;
}

int main()
{
static XGpio GPIOInstance_Ptr;
XGpioPs_Config*GpioConfigPtr;
XTmrCtr TimerInstancePtr;
int xStatus;
u32 Readstatus=0,OldReadStatus=0;
//u32 EffectiveAdress = 0xE000A000;
int iPinNumberEMIO = 54;
u32 uPinDirectionEMIO = 0x0;
// Input Pin
// Pin direction
u32 uPinDirection = 0x1;
int exit_flag,choice,internal_choice;
init_platform();
/* data = *(u32 *)(0x42800004);
print("OK \n");
data = *(u32 *)(0x41200004);
print("OK-1 \n");
*/
print("##### Application Starts #####\n\r");
print("\r\n");
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-1 :AXI GPIO Initialization
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
xStatus = XGpio_Initialize(&GPIOInstance_Ptr,XPAR_AXI_GPIO_1_DEVICE_ID);
if(XST_SUCCESS != xStatus)
print("GPIO INIT FAILED\n\r");
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-2 :AXI GPIO Set the Direction
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
XGpio_SetDataDirection(&GPIOInstance_Ptr, 1,1);
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-3 :AXI Timer Initialization
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
xStatus = XTmrCtr_Initialize(&TimerInstancePtr,XPAR_AXI_TIMER_1_DEVICE_ID);
if(XST_SUCCESS != xStatus)
print("TIMER INIT FAILED \n\r");
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-4 :Set Timer Handler
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
XTmrCtr_SetHandler(&TimerInstancePtr,
Timer_InterruptHandler,
&TimerInstancePtr);
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-5 :Setting timer Reset Value
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
XTmrCtr_SetResetValue(&TimerInstancePtr,
0, //Change with generic value
0xf0000000);
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-6 :Setting timer Option (Interrupt Mode And Auto Reload )
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
XTmrCtr_SetOptions(&TimerInstancePtr,
XPAR_AXI_TIMER_1_DEVICE_ID,
(XTC_INT_MODE_OPTION | XTC_AUTO_RELOAD_OPTION ));
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-7 :PS GPIO Intialization
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
GpioConfigPtr = XGpioPs_LookupConfig(XPAR_PS7_GPIO_1_DEVICE_ID);
if(GpioConfigPtr == NULL)
return XST_FAILURE;
xStatus = XGpioPs_CfgInitialize(&psGpioInstancePtr,
GpioConfigPtr,
GpioConfigPtr->BaseAddr);
if(XST_SUCCESS != xStatus)
print(" PS GPIO INIT FAILED \n\r");
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-8 :PS GPIO pin setting to Output
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
XGpioPs_SetDirectionPin(&psGpioInstancePtr, iPinNumber,uPinDirection);
XGpioPs_SetOutputEnablePin(&psGpioInstancePtr, iPinNumber,1);
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-9 :EMIO PIN Setting to Input port
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
XGpioPs_SetDirectionPin(&psGpioInstancePtr,
iPinNumberEMIO,uPinDirectionEMIO);
XGpioPs_SetOutputEnablePin(&psGpioInstancePtr, iPinNumberEMIO,0);
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-10 : SCUGIC interrupt controller Initialization
//Registration of the Timer ISR
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
xStatus=
ScuGicInterrupt_Init(XPAR_PS7_SCUGIC_1_DEVICE_ID,&TimerInstancePtr);
if(XST_SUCCESS != xStatus)
print(" :( SCUGIC INIT FAILED \n\r");
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
//Step-11 :User selection procedure to select and execute tests
//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
exit_flag = 0;
while(exit_flag != 1)
{
print(" SELECT the Operation from the Below Menu \r\n");
print("###################### Menu Starts ########################\r\n");
print("Press '1' to use NORMAL GPIO as an input (BTNU switch)\r\n");
print("Press '2' to use EMIO as an input (BTNR switch)\r\n");
print("Press any other key to Exit\r\n");
print(" ##################### Menu Ends #########################\r\n");
choice = inbyte();
printf("Selection : %c \r\n",choice);
internal_choice = 1;
switch(choice)
{
//~~~~~~~~~~~~~~~~~~~~~~~
// Use case for AXI GPIO
//~~~~~~~~~~~~~~~~~~~~~~~~
case '1':
exit_flag = 0;
print("Press Switch 'BTNU' push button on board \r\n");
print(" \r\n");
while(internal_choice != '0')
{
Readstatus = XGpio_DiscreteRead(&GPIOInstance_Ptr, 1);
if(1== Readstatus && 0 == OldReadStatus )
{
print("$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$\r\n");
print("BTNU PUSH Button pressed \n\r");
print("LED 'LD9' Turned OFF \r\n");
XGpioPs_WritePin(&psGpioInstancePtr,iPinNumber,0);
//Start Timer
XTmrCtr_Start(&TimerInstancePtr,0);
print("timer start \n\r");
//Wait For interrupt;
print("Wait for the Timer interrupt to tigger \r\n");
print("$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$\r\n");
print(" \r\n");
while(InterruptFlag != 1);
InterruptFlag = 0;
print(" ###########################################\r\n ");
print("Press '0' to go to Main Menu \n\r ");
print("Press any other key to remain in AXI GPIO Test \n\r ");
print(" ###########################################\r\n ");
internal_choice = inbyte();
printf("Select = %c \r\n",internal_choice);
if(internal_choice != '0')
{
print("Press Switch 'BTNU' push button on board \r\n");
}
}
OldReadStatus = Readstatus;
}
print(" \r\n");
print(" \r\n");
break;
case '2' :
//~~~~~~~~~~~~~~~~~~~~~~~
//Usecase for PS GPIO
//~~~~~~~~~~~~~~~~~~~~~~~~
exit_flag = 0;
print("Press Switch 'BTNR' push button on board \r\n");
print(" \r\n");
while(internal_choice != '0')
{
Readstatus = XGpioPs_ReadPin(&psGpioInstancePtr,
iPinNumberEMIO);
if(1== Readstatus && 0 == OldReadStatus )
{
print("$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$\r\n");
print("BTNR PUSH Button pressed \n\r");
print("LED 'LD9' Turned OFF \r\n");
XGpioPs_WritePin(&psGpioInstancePtr,iPinNumber,0);
//Start Timer
XTmrCtr_Start(&TimerInstancePtr,0);
print("timer start \n\r");
//Wait For interrupt;
print("Wait for the Timer interrupt to tigger \r\n");
print("$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$\r\n");
print(" \r\n");
while(InterruptFlag != 1);
InterruptFlag = 0;
print(" ###########################################\r\n ");
print("Press '0' to go to Main Menu \n\r ");
print("Press any other key to remain in EMIO Test \n\r ");
print(" ###########################################\r\n ");
internal_choice = inbyte();
printf("Select = %c \r\n",internal_choice);
if(internal_choice != '0')
{
print("Press Switch 'BTNR' push button on board \r\n");
}
}
OldReadStatus = Readstatus;
}
print(" \r\n");
print(" \r\n");
break;
default :
exit_flag = 1;
break;
}
}
print("\r\n");
print("***********\r\n");
print("BYE \r\n");
print("***********\r\n");
cleanup_platform();
return 0;
}
============================================================================================================

The above code is what gives Zedboard in document ZedBoard: Zynq-7000 AP SoC Concepts, Tools, and Techniques, in section Reference Designs / Tutorials. This code gives me errors in a series of "constant" as:

- XPAR_AXI_TIMER_1_DEVICE_ID
- XPAR_AXI_GPIO_1_DEVICE_ID

The error it complaining :#include "xtmrctr.h" and #include "xgpio.h"

 Why this error occurs? should I use the same version of my vivado and SDU according to my zedboard?

Thank you very much

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Sarah,

    For you first question about the two Devic ID's please refer to this post http://zedboard.org/content/zedboard-problem-code-sdk

    For the error compaining about xtmrctr.h and xgpio.h. Please refer to this detailed solution https://forums.xilinx.com/t5/Embedded-Development-Tools/Can-t-find-xgpio-h-xtmrctr-h/td-p/394271

    About your question of "should I use the same version of my vivado and SDU according to my zedboard?" the answer is yes, you should always use the same version of Vivado to version of SDK. For instance if you are using Vivado 2016.4 you should also be using SDK 2016.4

    --Josh