Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Booting Problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 542 views
  • Users 0 members are here
Related

Booting Problem

e14 Contributor
e14 Contributor over 10 years ago

Hiii every one,Here i have a problem with Zedboard booting from SDcard.Here I create all required files those are BOOT.bin using Xilinx SDK,,uImage.bin devicetree.dtb,,,,then after this i copied all these files to SDCard manually using ubuntu terminal...after this when i switch on the board,blue led also immulated but the booting process of linaro on  Zedboard never starts,,,,,so please help me how can i solve this problem

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    The most up-to-date solutions for ZedBoard with Linaro can be found on the Analog Devices Wiki here:

    https://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    sir when i am booting the zedboard it ids struct at this position


    U-Boot 2014.01 (Apr 19 2016 - 09:36:36)

    I2C:   ready
    Memory: ECC disabled
    DRAM:  512 MiB
    MMC:   zynq_sdhci: 0
    SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
    *** Warning - bad CRC, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   Gem.e000b000
    Hit any key to stop autoboot:  0
    Device: zynq_sdhci
    Manufacturer ID: 83
    OEM: 4e43
    Name: NCard
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 29.5 GiB
    Bus Width: 4-bit
    reading uEnv.txt
    ** Unable to read file uEnv.txt **
    Copying Linux from SD to RAM...
    reading uImage
    3724512 bytes read in 356 ms (10 MiB/s)
    reading devicetree.dtb
    9769 bytes read in 16 ms (595.7 KiB/s)
    ## Booting kernel from Legacy Image at 03000000 ...
       Image Name:   Linux-4.4.0-xilinx-g3c07939-dirt
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    3724448 Bytes = 3.6 MiB
       Load Address: 00008000
       Entry Point:  00008000
       Verifying Checksum ... OK
    ## Flattened Device Tree blob at 02a00000
       Booting using the fdt blob at 0x2a00000
       Loading Kernel Image ... OK
       Loading Device Tree to 1fb29000, end 1fb2e628 ... OK

    Starting kernel ...

    Booting Linux on physical CPU 0x0
    Linux version 4.4.0-xilinx-g3c07939-dirty (root@linux32) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #7 SMP PREEMPT Mon May 2 09:32:12 IST 2016
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    Machine model: Zynq Zed Development Board
    cma: Reserved 16 MiB at 0x1e800000
    Memory policy: Data cache writealloc
    PERCPU: Embedded 12 pages/cpu @5fbce000 s19328 r8192 d21632 u49152
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
    Kernel command line: console=ttyPS0,115200n8 root=/dev/ram rw initrd=0x00800000,16M earlyprintk mtdparts=physmap-flash.0:512K(nor-fsbl),512K(nor-u-boot),5M(nor-linux),9M(nor-user),1M(nor-scratch),-(nor-rootfs)
    PID hash table entries: 2048 (order: 1, 8192 bytes)
    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    Memory: 479228K/524288K available (5091K kernel code, 207K rwdata, 1788K rodata, 256K init, 224K bss, 28676K reserved, 16384K cma-reserved, 0K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0x60800000 - 0xff800000   (2544 MB)
        lowmem  : 0x40000000 - 0x60000000   ( 512 MB)
        pkmap   : 0x3fe00000 - 0x40000000   (   2 MB)
        modules : 0x3f000000 - 0x3fe00000   (  14 MB)
          .text : 0x40008000 - 0x406bff30   (6880 kB)
          .init : 0x406c0000 - 0x40700000   ( 256 kB)
          .data : 0x40700000 - 0x40733e60   ( 208 kB)
           .bss : 0x40733e60 - 0x4076bf34   ( 225 kB)
    Preemptible hierarchical RCU implementation.
            Build-time adjustment of leaf fanout to 32.
            RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2
    NR_IRQS:16 nr_irqs:16 16
    slcr mapped to 60800000
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at 60800100
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at 60808000, irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x8280 - 0x82d8
    CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    Brought up 2 CPUs
    SMP: Total of 2 processors activated (2664.03 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor ladder
    cpuidle: using governor menu
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x60880000
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    vgaarb: loaded
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    media: Linux media interface: v0.10
    Linux video capture interface: v2.00
    pps_core: LinuxPPS API ver. 1 registered
    pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    PTP clock support registered
    EDAC MC: Ver: 3.0.0
    Advanced Linux Sound Architecture Driver Initialized.
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    UDP hash table entries: 256 (order: 1, 8192 bytes)
    UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    NET: Registered protocol family 1
    RPC: Registered named UNIX socket transport module.
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    Trying to unpack rootfs image as initramfs...
    rootfs image is not initramfs (junk in compressed archive); looks like an initrd
    Freeing initrd memory: 16384K (40800000 - 41800000)
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    futex hash table entries: 512 (order: 3, 32768 bytes)
    jffs2: version 2.2. (NAND) (SUMMARY)  u00A9 2001-2006 Red Hat, Inc.
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
    dma-pl330 f8003000.dmac:        DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
    e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 143, base_baud = 3125000) is a xuartps
    console [ttyPS0] enabled
    xdevcfg f8007000.devcfg: ioremap 0xf8007000 to 6086c000
    [drm] Initialized drm 1.1.0 20060810
    brd: module loaded
    loop: module loaded
    m25p80 spi0.0: found s25fl256s1, expected n25q128a11
    m25p80 spi0.0: s25fl256s1 (32768 Kbytes)
    5 ofpart partitions found on MTD device spi0.0
    Creating 5 MTD partitions on "spi0.0":
    0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
    0x000000100000-0x000000600000 : "qspi-linux"
    0x000000600000-0x000000620000 : "qspi-device-tree"
    0x000000620000-0x000000c00000 : "qspi-rootfs"
    0x000000c00000-0x000001000000 : "qspi-bitstream"
    CAN device driver interface
    libphy: MACB_mii_bus: probed
    macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 146 (00:0a:35:00:01:22)
    macb e000b000.ethernet eth0: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=e000b000.etherne:00, irq=-1)
    e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
    e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    ehci-pci: EHCI PCI platform driver
    usbcore: registered new interface driver usb-storage
    mousedev: PS/2 mouse device common for all mice
    i2c /dev entries driver

    will you please help me sir